menu "Controller"
config OS_USING_NIMBLE_CONTROLLER
    bool "Indicates that NimBLE controller is present. The default value forthis setting shall not be overriden."
    default y

    if OS_USING_NIMBLE_CONTROLLER
		config MYNEWT_VAL_BLE_CONTROLLER
		    int 
		    default 1


		config NIMBLE_CFG_CONTROLLER
		    int 
			default 0 if !OS_USING_NIMBLE_CONTROLLER
		    default 1 if OS_USING_NIMBLE_CONTROLLER


		config MYNEWT_VAL_BLE_CTLR_THREAD_STACK_SIZE
		    int "BLE controller thread stack size"
			default 2048


		config MYNEWT_VAL_BLE_CTLR_THREAD_PRIORITY
		    int "BLE controller thread priority"
			default 4


		# config MYNEWT_VAL_BLE_HW_WHITELIST_ENABLE
		#     int "Used to enable hardware white list"
		#     default 1
        config BLE_HW_WHITELIST_ENABLE
            bool "Used to enable hardware white list"
			default n if BLE_LL_CFG_FEAT_LL_EXT_ADV
            default y
        config MYNEWT_VAL_BLE_HW_WHITELIST_ENABLE
            int
            default 0 if !BLE_HW_WHITELIST_ENABLE
            default 1 if BLE_HW_WHITELIST_ENABLE


        # config MYNEWT_VAL_BLE_LL_SYSVIEW
        #    int "Enable SystemView tracing module for controller."
        #    default 0
        config BLE_LL_SYSVIEW
            bool "Enable SystemView tracing module for controller."
            default n
        config MYNEWT_VAL_BLE_LL_SYSVIEW
            int 
            default 0 if !BLE_LL_SYSVIEW
            default 1 if BLE_LL_SYSVIEW

		config MYNEWT_VAL_BLE_LL_PRIO
		    int "The priority of the LL task"
		    default 0


		config MYNEWT_VAL_BLE_LL_SCA
		    int "Sleep clock accuracy of our device (in ppm)"
		    default MYNEWT_VAL_BLE_LL_OUR_SCA

		config MYNEWT_VAL_BLE_LL_TX_PWR_DBM
		    int "Transmit power level."
		    default 0

		config MYNEWT_VAL_BLE_LL_NUM_COMP_PKT_ITVL_MS
		    int "Determines the interval at which the controller will send the number of completed packets event to the host"
		    default 2000

		    help 
				Determines the interval at which the controller will send the number of completed packets event to the host. Rate is in milliseconds.

		config MYNEWT_VAL_BLE_LL_MFRG_ID
		    hex "Manufacturer ID. Should be set to unique ID per manufacturer."
		    default 0xFFFF

		config MYNEWT_VAL_BLE_LL_NUM_SCAN_DUP_ADVS
		    int "The number of duplicate advertisers stored."
		    default 8

		config MYNEWT_VAL_BLE_LL_NUM_SCAN_RSP_ADVS
		    int "The number of advertisers from which we have heard a scan response"
		    default 8
		    help 
				The number of advertisers from which we have heard a scan response. Prevents sending duplicate events to host.

		config MYNEWT_VAL_BLE_LL_WHITELIST_SIZE
		    int "Size of the LL whitelist."
		    default 8

		config MYNEWT_VAL_BLE_LL_RESOLV_LIST_SIZE
		    int "Size of the resolving list."
		    default 4

		config MYNEWT_VAL_BLE_LL_MAX_PKT_SIZE
		    int "The maximum PDU size that can be sent/received"
		    default 251

		config MYNEWT_VAL_BLE_LL_SUPP_MAX_RX_BYTES
		    int "The maximum supported received PDU size"
		    default MYNEWT_VAL_BLE_LL_MAX_PKT_SIZE

		config MYNEWT_VAL_BLE_LL_SUPP_MAX_TX_BYTES
		    int "The maximum supported transmit PDU size"
		    default MYNEWT_VAL_BLE_LL_MAX_PKT_SIZE

		config MYNEWT_VAL_BLE_LL_CONN_INIT_MAX_TX_BYTES
		    int "Used to set the initial maximum transmit PDU size in a connection"
		    default 27
		    help 
				Used to set the initial maximum transmit PDU size in a connection. If this is set to a value greater than 27, the controller will automatically attempt to do the data length update procedure. The host can always tell the controller to update this value.

		config MYNEWT_VAL_BLE_LL_CONN_INIT_SLOTS
		    int "This is the number of 'slots' allocated to a connection when scheduling connections"
		    default 4
		    help 
				This is the number of 'slots' allocated to a connection when scheduling connections. Each slot is 1.25 msecs long. Note that a connection event may last longer than the number of slots allocated here and may also end earlier (depending on when the next scheduled event occurs and how much data needs to be transferred in the connection). However, you will be guaranteed that a connection event will be given this much time, if needed. Consecutively scheduled items will be at least this far apart

		config MYNEWT_VAL_BLE_LL_CONN_INIT_MIN_WIN_OFFSET
		    int "This is the minimum number of 'slots' for WindowOffset value used for CONNECT_IND when creating new connection as a master"
		    default 0
		    help 
				This is the minimum number of 'slots' for WindowOffset value used for CONNECT_IND when creating new connection as a master. Each slot is 1.25 msecs long. Increasing this value will delay first connection event after connection is created. However, older TI CC254x controllers cannot change connection parameters later if WindowOffset was set to 0 in CONNECT_IND. To ensure interoperability with such devices set this value to 2 (or more).

		config MYNEWT_VAL_BLE_LL_STRICT_CONN_SCHEDULING
		    int "Forces the scheduler on a central to schedule connections in fixed time intervals called periods"
		    default 0
		    help 
				Forces the scheduler on a central to schedule connections in fixed time intervals called periods. If set to 0, the scheduler is not forced to do this. If set to 1, the scheduler will only schedule connections at period boundaries. See comments in ble_ll_sched.h for more details.

		config MYNEWT_VAL_BLE_LL_ADD_STRICT_SCHED_PERIODS
		    int "The number of additional periods that will be allocated for strict scheduling"
		    default 0
		    help 
				The number of additional periods that will be allocated for strict scheduling. The total # of periods allocated for strict scheduling will be equal to the number of connections plus this number.

		config MYNEWT_VAL_BLE_LL_USECS_PER_PERIOD
		    int "The number of usecs per period."
		    default 3250

		config MYNEWT_VAL_BLE_LL_RNG_BUFSIZE
		    int "The number of random bytes that the link layer will try to always have available for the host to use"
		    default 32
		    help 
				The number of random bytes that the link layer will try to always have available for the host to use. Decreasing this value may cause host delays if the host needs lots of random material often.

		config MYNEWT_VAL_BLE_LL_RFMGMT_ENABLE_TIME
		    int "Time required for radio and/or related components to be fully enabled before any request from LL is sent"
		    default MYNEWT_VAL_BLE_XTAL_SETTLE_TIME
		    help 
				Time required for radio and/or related components to be fully enabled before any request from LL is sent. This value is used by rfmgmt to enable PHY in advance, before request from LL is made. It depends on radio driver selected and may also depend on hardware used: - nrf51 - time required for XTAL to settle - nrf52 - time required for XTAL to settle Value is specified in microseconds. If set to 0, rfmgmt keeps PHY enabled all the time.


        # config MYNEWT_VAL_BLE_LL_CFG_FEAT_LE_ENCRYPTION
        #    int This option enables/disables encryption support in the controller. This option saves both both code and RAM.
        #    default 1
        config BLE_LL_CFG_FEAT_LE_ENCRYPTION
            bool "This option enables/disables encryption support in the controller"
            default y
            help
                This option enables/disables encryption support in the controller. This option saves both both code and RAM.
        config MYNEWT_VAL_BLE_LL_CFG_FEAT_LE_ENCRYPTION
            int 
            default 0 if !BLE_LL_CFG_FEAT_LE_ENCRYPTION
            default 1 if BLE_LL_CFG_FEAT_LE_ENCRYPTION


        # config MYNEWT_VAL_BLE_LL_CFG_FEAT_CONN_PARAM_REQ
        #    int This option enables/disables the connection parameter request procedure.  This is implemented in the controller but is disabled by default.
        #    default 1
        config BLE_LL_CFG_FEAT_CONN_PARAM_REQ
            bool "This option enables/disables the connection parameter request procedure"
            default y
            help
                This option enables/disables the connection parameter request procedure.  This is implemented in the controller but is disabled by default.
        config MYNEWT_VAL_BLE_LL_CFG_FEAT_CONN_PARAM_REQ
            int 
            default 0 if !BLE_LL_CFG_FEAT_CONN_PARAM_REQ
            default 1 if BLE_LL_CFG_FEAT_CONN_PARAM_REQ


        # config MYNEWT_VAL_BLE_LL_CFG_FEAT_SLAVE_INIT_FEAT_XCHG
        #    int This option allows a slave to initiate the feature exchange procedure.  This feature is implemented but currently has no impact on code or ram size
        #    default 1
        config BLE_LL_CFG_FEAT_SLAVE_INIT_FEAT_XCHG
            bool "This option allows a slave to initiate the feature exchange procedure"
            default y
            help
                This option allows a slave to initiate the feature exchange procedure.  This feature is implemented but currently has no impact on code or ram size
        config MYNEWT_VAL_BLE_LL_CFG_FEAT_SLAVE_INIT_FEAT_XCHG
            int 
            default 0 if !BLE_LL_CFG_FEAT_SLAVE_INIT_FEAT_XCHG
            default 1 if BLE_LL_CFG_FEAT_SLAVE_INIT_FEAT_XCHG


        config MYNEWT_VAL_BLE_LL_CFG_FEAT_LE_PING
           int "This option allows a controller to send/receive LE pings. Currently, this feature is not implemented by the controller so turning it on or off has no effect."
           default MYNEWT_VAL_BLE_LL_CFG_FEAT_LE_ENCRYPTION


        # config MYNEWT_VAL_BLE_LL_CFG_FEAT_DATA_LEN_EXT
        #    int This option enables/disables the data length update procedure in the controller. If enabled, the controller is allowed to change the size of tx/rx pdu's used in a connection. This option has only minor impact on code size and non on RAM.
        #    default 1
        config BLE_LL_CFG_FEAT_DATA_LEN_EXT
            bool "This option enables/disables the data length update procedure in the controller"
            default y
            help
                This option enables/disables the data length update procedure in the controller. If enabled, the controller is allowed to change the size of tx/rx pdu's used in a connection. This option has only minor impact on code size and non on RAM.
        config MYNEWT_VAL_BLE_LL_CFG_FEAT_DATA_LEN_EXT
            int 
            default 0 if !BLE_LL_CFG_FEAT_DATA_LEN_EXT
            default 1 if BLE_LL_CFG_FEAT_DATA_LEN_EXT


        # config MYNEWT_VAL_BLE_LL_CFG_FEAT_LL_PRIVACY
        #    int "This option is used to enable/disable LL privacy."
        #    default 1
        config BLE_LL_CFG_FEAT_LL_PRIVACY
            bool "This option is used to enable/disable LL privacy."
            default y
        config MYNEWT_VAL_BLE_LL_CFG_FEAT_LL_PRIVACY
            int 
            default 0 if !BLE_LL_CFG_FEAT_LL_PRIVACY
            default 1 if BLE_LL_CFG_FEAT_LL_PRIVACY


        # config MYNEWT_VAL_BLE_LL_CFG_FEAT_LE_CSA2
        #    int "This option is used to enable/disable support for LE Channel Selection Algorithm #2."
        #    default 0
        config BLE_LL_CFG_FEAT_LE_CSA2
            bool "This option is used to enable/disable support for LE Channel Selection Algorithm #2."
			default y if BLE_LL_CFG_FEAT_LL_EXT_ADV
            default n
        config MYNEWT_VAL_BLE_LL_CFG_FEAT_LE_CSA2
            int 
            default 0 if !BLE_LL_CFG_FEAT_LE_CSA2
            default 1 if BLE_LL_CFG_FEAT_LE_CSA2


        # config MYNEWT_VAL_BLE_LL_CFG_FEAT_LE_2M_PHY
        #    int "This option is used to enable/disable support for the 2Mbps PHY."
        #    default 0
        config BLE_LL_CFG_FEAT_LE_2M_PHY
            bool "This option is used to enable/disable support for the 2Mbps PHY."
            default n
        config MYNEWT_VAL_BLE_LL_CFG_FEAT_LE_2M_PHY
            int 
            default 0 if !BLE_LL_CFG_FEAT_LE_2M_PHY
            default 1 if BLE_LL_CFG_FEAT_LE_2M_PHY


        # config MYNEWT_VAL_BLE_LL_CFG_FEAT_LE_CODED_PHY
        #    int "This option is used to enable/disable support for the coded PHY."
        #    default 0
        config BLE_LL_CFG_FEAT_LE_CODED_PHY
            bool "This option is used to enable/disable support for the coded PHY."
            default n
        config MYNEWT_VAL_BLE_LL_CFG_FEAT_LE_CODED_PHY
            int 
            default 0 if !BLE_LL_CFG_FEAT_LE_CODED_PHY
            default 1 if BLE_LL_CFG_FEAT_LE_CODED_PHY


        # config MYNEWT_VAL_BLE_LL_CFG_FEAT_LL_EXT_ADV
		# 	int "This option is used to enable/disable support for Extended Advertising Feature. That means extended scanner, advertiser and connect."
		# 	default MYNEWT_VAL_BLE_EXT_ADV
		config BLE_LL_CFG_FEAT_LL_EXT_ADV
            bool "This option is used to enable/disable support for Extended Advertising Feature. That means extended scanner, advertiser and connect."
            default n if !BLE_EXT_ADV
			default y if BLE_EXT_ADV
        config MYNEWT_VAL_BLE_LL_CFG_FEAT_LL_EXT_ADV
            int
            default 0 if !BLE_LL_CFG_FEAT_LL_EXT_ADV
            default 1 if BLE_LL_CFG_FEAT_LL_EXT_ADV
		   

        # config MYNEWT_VAL_BLE_LL_CFG_FEAT_LL_PERIODIC_ADV
		# 	int "This option is used to enable/disable support for Periodic Advertising Feature."
		# 	default MYNEWT_VAL_BLE_PERIODIC_ADV
		config BLE_LL_CFG_FEAT_LL_PERIODIC_ADV
            bool "This option is used to enable/disable support for Periodic Advertising Feature."
            default n if !BLE_PERIODIC_ADV
			default y if BLE_PERIODIC_ADV
        config MYNEWT_VAL_BLE_LL_CFG_FEAT_LL_PERIODIC_ADV
            int
            default 0 if !BLE_LL_CFG_FEAT_LL_PERIODIC_ADV
            default 1 if BLE_LL_CFG_FEAT_LL_PERIODIC_ADV


        config MYNEWT_VAL_BLE_LL_CFG_FEAT_LL_PERIODIC_ADV_SYNC_CNT
			int "This option is used to configure number of supported periodic syncs."
			default MYNEWT_VAL_BLE_MAX_PERIODIC_SYNCS


        config MYNEWT_VAL_BLE_LL_CFG_FEAT_LL_PERIODIC_ADV_SYNC_LIST_CNT
			int "Size of Periodic Advertiser sync list."
			default MYNEWT_VAL_BLE_MAX_PERIODIC_SYNCS


        # config MYNEWT_VAL_BLE_LL_CFG_FEAT_LL_PERIODIC_ADV_SYNC_TRANSFER
		# 	int "This option is use to enable/disable support for Periodic Advertising Sync Transfer Feature."
		# 	default MYNEWT_VAL_BLE_PERIODIC_ADV_SYNC_TRANSFER
		config BLE_LL_CFG_FEAT_LL_PERIODIC_ADV_SYNC_TRANSFER
            bool "This option is use to enable/disable support for Periodic Advertising Sync Transfer Feature."
            default n if !BLE_PERIODIC_ADV_SYNC_TRANSFER
			default y if BLE_PERIODIC_ADV_SYNC_TRANSFER
        config MYNEWT_VAL_BLE_LL_CFG_FEAT_LL_PERIODIC_ADV_SYNC_TRANSFER
            int
            default 0 if !BLE_LL_CFG_FEAT_LL_PERIODIC_ADV_SYNC_TRANSFER
            default 1 if BLE_LL_CFG_FEAT_LL_PERIODIC_ADV_SYNC_TRANSFER


        # config MYNEWT_VAL_BLE_LL_CFG_FEAT_CTRL_TO_HOST_FLOW_CONTROL
        #    int Enable controller-to-host flow control support. This allows host to limit number of ACL packets sent at once from controller to avoid congestion on HCI transport if feature is also supported by host.
        #    default 0
        config BLE_LL_CFG_FEAT_CTRL_TO_HOST_FLOW_CONTROL
            bool "Enable controller-to-host flow control support"
            default n
            help
                Enable controller-to-host flow control support. This allows host to limit number of ACL packets sent at once from controller to avoid congestion on HCI transport if feature is also supported by host.
        config MYNEWT_VAL_BLE_LL_CFG_FEAT_CTRL_TO_HOST_FLOW_CONTROL
            int 
            default 0 if !BLE_LL_CFG_FEAT_CTRL_TO_HOST_FLOW_CONTROL
            default 1 if BLE_LL_CFG_FEAT_CTRL_TO_HOST_FLOW_CONTROL


        # config MYNEWT_VAL_BLE_LL_CFG_FEAT_LL_SCA_UPDATE
        #    int "This option is used to enable/disable support for SCA update procedure"
        #    default 0
        config BLE_LL_CFG_FEAT_LL_SCA_UPDATE
            bool "This option is used to enable/disable support for SCA update procedure"
            default n
        config MYNEWT_VAL_BLE_LL_CFG_FEAT_LL_SCA_UPDATE
            int 
            default 0 if !BLE_LL_CFG_FEAT_LL_SCA_UPDATE
            default 1 if BLE_LL_CFG_FEAT_LL_SCA_UPDATE


        # config MYNEWT_VAL_BLE_LL_CFG_FEAT_LL_ISO
		# 	int "This option is used to enable/disable support for LE Isochronous Channels as per Bluetooth v5.2 channels"
		# 	default MYNEWT_VAL_BLE_ISO
		config BLE_LL_CFG_FEAT_LL_ISO
            bool "This option is used to enable/disable support for LE Isochronous Channels as per Bluetooth v5.2 channels"
            default n if !BLE_ISO
			default y if BLE_ISO
        config MYNEWT_VAL_BLE_LL_CFG_FEAT_LL_ISO
            int
            default 0 if !BLE_LL_CFG_FEAT_LL_ISO
            default 1 if BLE_LL_CFG_FEAT_LL_ISO


        # config MYNEWT_VAL_BLE_LL_CFG_FEAT_LL_ISO_TEST
		# 	int "This option is used to enable/disbale test commands for ISO support"
		# 	default MYNEWT_VAL_BLE_ISO_TEST
		config BLE_LL_CFG_FEAT_LL_ISO_TEST
            bool "This option is used to enable/disbale test commands for ISO support"
            default n if !BLE_ISO_TEST
			default y if BLE_ISO_TEST
        config MYNEWT_VAL_BLE_LL_CFG_FEAT_LL_ISO_TEST
            int
            default 0 if !BLE_LL_CFG_FEAT_LL_ISO_TEST
            default 1 if BLE_LL_CFG_FEAT_LL_ISO_TEST


		config MYNEWT_VAL_BLE_LL_EXT_ADV_AUX_PTR_CNT
		    int "This option configure a max number of scheduled outstanding auxiliary packets for receive on secondary advertising channel"
			default 5 if BLE_LL_CFG_FEAT_LL_EXT_ADV
		    default 0

		    help 
				This option configure a max number of scheduled outstanding auxiliary packets for receive on secondary advertising channel.

		# config MYNEWT_VAL_BLE_PUBLIC_DEV_ADDR
		#     int "Allows the target or app to override the public device address used by the controller"
		#     default (uint8_t[6]){0x00, 0x00, 0x00, 0x00, 0x00, 0x00}
		#     help 
		# 		Allows the target or app to override the public device address used by the controller. If all zero, the controller will attempt to retrieve the public device address from its chip specific location. If non-zero, this address will be used.

		# config MYNEWT_VAL_BLE_LL_DTM
		#     int "Enables HCI Test commands needed for Bluetooth SIG certification"
		#     default MYNEWT_VAL_BLE_LL_DIRECT_TEST_MODE
		config BLE_LL_DTM
            bool "Enables HCI Test commands needed for Bluetooth SIG certification"
            default n if !BLE_LL_DIRECT_TEST_MODE
			default y if BLE_LL_DIRECT_TEST_MODE
        config MYNEWT_VAL_BLE_LL_DTM
            int
            default 0 if !BLE_LL_DTM
            default 1 if BLE_LL_DTM


		# config MYNEWT_VAL_BLE_LL_DTM_EXTENSIONS
		#     int "Enables non-standard extensions to HCI test commands"
		#     default 0
		#     help 
		# 		 Enables non-standard extensions to HCI test commands. Once enabled,  HCI_LE_Transmitter_Test accepts extra parameters in addition to  those defined in Core specification    interval (2 octets)   interval between packets (usecs), overrides                          standard interval    pkt_count (2 octets)  number of packets to transmit, controller                          will automatically stop sending packets                          after given number of packets was sent  Setting either of these parameters to 0 will configure for default  behavior, as per Core specification.  If specified interval is shorter then allowed by specification it  will be ignored.  Extended parameters shall immediately follow standard parameters.  Controller can accept both standard and extended version of command  depending on specified HCI command length.
		config BLE_LL_DTM_EXTENSIONS
            bool "Enables non-standard extensions to HCI test commands"
            default n
			help 
				 Enables non-standard extensions to HCI test commands. Once enabled,  HCI_LE_Transmitter_Test accepts extra parameters in addition to  those defined in Core specification    interval (2 octets)   interval between packets (usecs), overrides                          standard interval    pkt_count (2 octets)  number of packets to transmit, controller                          will automatically stop sending packets                          after given number of packets was sent  Setting either of these parameters to 0 will configure for default  behavior, as per Core specification.  If specified interval is shorter then allowed by specification it  will be ignored.  Extended parameters shall immediately follow standard parameters.  Controller can accept both standard and extended version of command  depending on specified HCI command length.
        config MYNEWT_VAL_BLE_LL_DTM_EXTENSIONS
            int
            default 0 if !BLE_LL_DTM_EXTENSIONS
            default 1 if BLE_LL_DTM_EXTENSIONS


		# config MYNEWT_VAL_BLE_LL_VND_EVENT_ON_ASSERT
		#     int "This options enables controller to send a vendor-specific event on an assertion in controller code"
		#     default 0
		#     help 
		# 		This options enables controller to send a vendor-specific event on an assertion in controller code. The event contains file name and line number where assertion occured.
		config BLE_LL_VND_EVENT_ON_ASSERT
            bool "This options enables controller to send a vendor-specific event on an assertion in controller code"
			default y if !BLE_HOST
            default n
			help 
				This options enables controller to send a vendor-specific event on an assertion in controller code. The event contains file name and line number where assertion occured.
        config MYNEWT_VAL_BLE_LL_VND_EVENT_ON_ASSERT
            int
            default 0 if !BLE_LL_VND_EVENT_ON_ASSERT
            default 1 if BLE_LL_VND_EVENT_ON_ASSERT


		config MYNEWT_VAL_BLE_LL_SYSINIT_STAGE
		    int "Sysinit stage for the NimBLE controller."
		    default 250


		config MYNEWT_VAL_BLE_LL_DEBUG_GPIO_HCI_CMD
		    int "GPIO pin number to debug HCI commands flow"
		    default -1

		    help 
				GPIO pin number to debug HCI commands flow. Pin is set to high state when HCI command is being processed.

		config MYNEWT_VAL_BLE_LL_DEBUG_GPIO_HCI_EV
		    int "GPIO pin number to debug HCI events flow. Pin is set to high state when HCI event is being sent."
		    default -1


		config MYNEWT_VAL_BLE_LL_DEBUG_GPIO_SCHED_RUN
		    int "GPIO pin number to debug scheduler running (on timer)"
		    default -1

		    help 
				GPIO pin number to debug scheduler running (on timer). Pin is set to high state while scheduler is running.

		config MYNEWT_VAL_BLE_LL_DEBUG_GPIO_SCHED_ITEM_CB
		    int "GPIO pin number to debug scheduler item execution times"
		    default -1

		    help 
				GPIO pin number to debug scheduler item execution times. Pin is set to high state while item is executed.

		config MYNEWT_VAL_BLE_LL_SCHED_AUX_MAFS_DELAY
		    int "Additional delay [us] between last ADV_EXT_IND and AUX_ADV_IND PDUs when scheduling extended advertising event"
		    default 0

		    help 
				Additional delay [us] between last ADV_EXT_IND and AUX_ADV_IND PDUs when scheduling extended advertising event. This extends T_MAFS.

		config MYNEWT_VAL_BLE_LL_SCHED_AUX_CHAIN_MAFS_DELAY
		    int "Additional delay [us] between consecutive AUX_CHAIN_IND PDUs when scheduling extended or periodic advertising event"
		    default 0

		    help 
				Additional delay [us] between consecutive AUX_CHAIN_IND PDUs when scheduling extended or periodic advertising event. This extends T_MAFS.

		config MYNEWT_VAL_BLE_LL_SCHED_SCAN_AUX_PDU_LEN
		    int "This is expected PDU len for AUX_ADV_IND and subsequent AUX_CHAIN_IND"
		    default 41

		    help 
				This is expected PDU len for AUX_ADV_IND and subsequent AUX_CHAIN_IND. When scheduling scan scheduler will reserve time for receiving this amount of time. Setting this to high value improves reception of large PDUs but results in wasting scheduler space when receiving small PDUs only. On the other hand too low value can result in not being able to scan whole PDU due to being preempted by next scheduled item. By default size matching legacy ADV_IND PDU payload is used: ExtHeader (Flags, AdvA, ADI) + 31 bytes of data.

		config MYNEWT_VAL_BLE_LL_SCHED_SCAN_SYNC_PDU_LEN
		    int "This is expected PDU len for AUX_SYNC_IND and subsequent AUX_CHAIN_IND"
		    default 32

		    help 
				This is expected PDU len for AUX_SYNC_IND and subsequent AUX_CHAIN_IND. When scheduling scan scheduler will reserve time for receiving this amount of time. Setting this to high value improves reception of large PDUs but results in wasting scheduler space when receiving small PDUs only. On the other hand too low value can result in not being able to scan whole PDU due to being preempted by next scheduled item. By default size matching PDU with legacy data size is used: ExtHeader + 31 bytes of data.

		config MYNEWT_VAL_BLE_LL_DIRECT_TEST_MODE
		    int "use BLE_LL_DTM instead"
		    default 0


		config MYNEWT_VAL_BLE_XTAL_SETTLE_TIME
		    int "use BLE_LL_RFMGMT_ENABLE_TIME instead"
		    default 0


		config MYNEWT_VAL_BLE_LL_OUR_SCA
		    int "use BLE_LL_SCA instead"
		    default 60


		config MYNEWT_VAL_BLE_DEVICE
		    int "Superseded by BLE_CONTROLLER"
		    default 1


		config MYNEWT_VAL_BLE_LP_CLOCK
		    int "Superseded by BLE_CONTROLLER"
		    default 1


		config MYNEWT_VAL_BLE_NUM_COMP_PKT_RATE
		    int "Superseded by BLE_LL_NUM_COMP_PKT_ITVL_MS"
		    # default (2 * OS_TICKS_PER_SEC)
			default 200

		config MYNEWT_VAL_BLE_LL_MASTER_SCA
		    int "use BLE_LL_SCA instead"
		    default 4


    endif
endmenu