config BLE_HOST_MESH
    bool "Indicates that NimBLE mesh is present."
    default n

    if BLE_HOST_MESH

        # config MYNEWT_VAL_BLE_MESH_PROV
        #    int Enable provisioning. It is automatically enabled whenever BLE_MESH_PB_ADV or BLE_MESH_PB_GATT is set.
        #    default 1
        config BLE_MESH_PROV
            bool "Enable provisioning"
			default y if BLE_MESH_PB_GATT
			default y if BLE_MESH_PB_ADV
            default y
            help
                Enable provisioning. It is automatically enabled whenever BLE_MESH_PB_ADV or BLE_MESH_PB_GATT is set.
        config MYNEWT_VAL_BLE_MESH_PROV
            int 
            default 0 if !BLE_MESH_PROV
            default 1 if BLE_MESH_PROV


        # config MYNEWT_VAL_BLE_MESH_PB_ADV
        #    int "Enable this option to allow the device to be provisioned over the advertising bearer."
        #    default 1
        config BLE_MESH_PB_ADV
            bool "Enable this option to allow the device to be provisioned over the advertising bearer."
            default y
        config MYNEWT_VAL_BLE_MESH_PB_ADV
            int 
            default 0 if !BLE_MESH_PB_ADV
            default 1 if BLE_MESH_PB_ADV


        # config MYNEWT_VAL_BLE_MESH_PROVISIONER
        #    int "Enable this option to have support for provisioning remote devices."
        #    default 0
        config BLE_MESH_PROVISIONER
            bool "Enable this option to have support for provisioning remote devices."
            default n
        config MYNEWT_VAL_BLE_MESH_PROVISIONER
            int 
            default 0 if !BLE_MESH_PROVISIONER
            default 1 if BLE_MESH_PROVISIONER

		config MYNEWT_VAL_BLE_MESH_NODE_COUNT
		    int "This option specifies how many nodes each network can at most save in the provisioning database"
		    default 1

		    help 
				This option specifies how many nodes each network can at most save in the provisioning database. Range 1-4096


        # config MYNEWT_VAL_BLE_MESH_PROXY
        #    int "Enable proxy. This is automatically set whenever BLE_MESH_PB_GATT or BLE_MESH_GATT_PROXY is set."
        #    default 0
        config BLE_MESH_PROXY
            bool "Enable proxy. This is automatically set whenever BLE_MESH_PB_GATT or BLE_MESH_GATT_PROXY is set."
			default y if BLE_MESH_GATT_PROXY
			default y if BLE_MESH_PB_GATT
            default n
        config MYNEWT_VAL_BLE_MESH_PROXY
            int 
            default 0 if !BLE_MESH_PROXY
            default 1 if BLE_MESH_PROXY


        # config MYNEWT_VAL_BLE_MESH_PB_GATT
        #    int "Enable this option to allow the device to be provisioned over the GATT bearer."
        #    default 1
        config BLE_MESH_PB_GATT
            bool "Enable this option to allow the device to be provisioned over the GATT bearer."
            default y
        config MYNEWT_VAL_BLE_MESH_PB_GATT
            int 
            default 0 if !BLE_MESH_PB_GATT
            default 1 if BLE_MESH_PB_GATT

		# config MYNEWT_VAL_BLE_MESH_GATT_PROXY
		#     int "This option enables support for the Mesh GATT Proxy Service, i"
		#     default 1
		#     help 
		# 		This option enables support for the Mesh GATT Proxy Service, i.e. the ability to act as a proxy between a Mesh GATT Client and a Mesh network.
		config BLE_MESH_GATT_PROXY
		    bool "This option enables support for the Mesh GATT Proxy Service."
		    default y
		    help 
				This option enables support for the Mesh GATT Proxy Service, i.e. the ability to act as a proxy between a Mesh GATT Client and a Mesh network.
		config MYNEWT_VAL_BLE_MESH_GATT_PROXY
            int 
            default 0 if !BLE_MESH_GATT_PROXY
            default 1 if BLE_MESH_GATT_PROXY

		config MYNEWT_VAL_BLE_MESH_NODE_ID_TIMEOUT
		    int "This option determines for how long the local node advertises using Node Identity"
		    default 60

		    help 
				This option determines for how long the local node advertises using Node Identity. The given value is in seconds. The specification limits this to 60 seconds, and implies that to be the appropriate value as well, so just leaving this as the default is the safest option.

		config MYNEWT_VAL_BLE_MESH_PROXY_FILTER_SIZE
		    int ""
		    default 1


		config MYNEWT_VAL_BLE_MESH_SUBNET_COUNT
		    int "This option specifies how many subnets a Mesh network can participate in at the same time."
		    default 1


		config MYNEWT_VAL_BLE_MESH_APP_KEY_COUNT
		    int "This option specifies how many application keys the device can store per network."
		    default 1


		config MYNEWT_VAL_BLE_MESH_MODEL_KEY_COUNT
		    int "This option specifies how many application keys each model can  at most be bound to."
		    default 1


		config MYNEWT_VAL_BLE_MESH_MODEL_GROUP_COUNT
		    int "This option specifies how many group addresses each model can at most be subscribed to."
		    default 1


		config MYNEWT_VAL_BLE_MESH_LABEL_COUNT
		    int "This option specifies how many Label UUIDs can be stored."
		    default 1


		config MYNEWT_VAL_BLE_MESH_CRPL
		    int "This options specifies the maximum capacity of the replay protection list"
		    default 10

		    help 
				This options specifies the maximum capacity of the replay protection list. This option is similar to the network message cache size, but has a different purpose.

		config MYNEWT_VAL_BLE_MESH_ADV_TASK_PRIO
		    int "Advertising task prio (FIXME)"
		    default 9


		config MYNEWT_VAL_BLE_MESH_MSG_CACHE_SIZE
		    int "Number of messages that are cached for the network"
		    default 10

		    help 
				Number of messages that are cached for the network. This description prevent unnecessary decryption operations and unnecessary relays. This option is similar to the replay protection list, but has a different purpose.

		config MYNEWT_VAL_BLE_MESH_ADV_BUF_COUNT
		    int "Number of advertising buffers available"
		    default 6

		    help 
				Number of advertising buffers available. This should be chosen based on what kind of features the local node shoule have. E.g. a relay will perform better the more buffers it has. Another thing to consider is outgoing segmented messages. There must be at least three more advertising buffers than the maximum supported outgoing segment count (BT_MESH_TX_SEG_MAX).

		config MYNEWT_VAL_BLE_MESH_IVU_DIVIDER
		    int "When the IV Update state enters Normal operation or IV Update in Progress, we need to keep track of how many hours has passed in the state, since the specification requires us to remain in the state at least for 96 hours (Update in Progress has an additional upper limit of 144 hours)"
		    default 4

		    help 
				When the IV Update state enters Normal operation or IV Update in Progress, we need to keep track of how many hours has passed in the state, since the specification requires us to remain in the state at least for 96 hours (Update in Progress has an additional upper limit of 144 hours).

		config MYNEWT_VAL_BLE_MESH_TX_SEG_MSG_COUNT
		    int "Maximum number of simultaneous outgoing multi-segment and/or reliable messages."
		    default 4


		config MYNEWT_VAL_BLE_MESH_RX_SEG_MSG_COUNT
		    int "Maximum number of simultaneous incoming multi-segment and/or reliable messages."
		    default 2


		config MYNEWT_VAL_BLE_MESH_RX_SDU_MAX
		    int "Maximum incoming Upper Transport Access PDU length"
		    default 72

		    help 
				Maximum incoming Upper Transport Access PDU length. This determines also how many segments incoming segmented messages can have. Each segment can contain 12 bytes, so this value should be set to a multiple of 12 to avoid wasted memory. The minimum requirement is 2 segments (24 bytes) whereas the maximum supported by the Mesh specification is 32 segments (384 bytes).

		config MYNEWT_VAL_BLE_MESH_TX_SEG_MAX
		    int "Maximum number of segments supported for outgoing messages"
		    default 3

		    help 
				Maximum number of segments supported for outgoing messages. This value should typically be fine-tuned based on what models the local node supports, i.e. what's the largest message payload that the node needs to be able to send. This value affects memory and call stack consumption, which is why the default is lower than the maximum that the specification would allow (32 segments).

		config MYNEWT_VAL_BLE_MESH_SEG_RETRANSMIT_ATTEMPTS
		    int "Number of retransmit attempts (after the initial transmit) per segment"
		    default 4


		config MYNEWT_VAL_BLE_MESH_RELAY
		    int "Support for acting as a Mesh Relay Node."
		    default 0



        # config MYNEWT_VAL_BLE_MESH_LOW_POWER
        #    int "Enable this option to be able to act as a Low Power Node."
        #    default 0
        config BLE_MESH_LOW_POWER
            bool "Enable this option to be able to act as a Low Power Node."
            default n
        config MYNEWT_VAL_BLE_MESH_LOW_POWER
            int 
            default 0 if !BLE_MESH_LOW_POWER
            default 1 if BLE_MESH_LOW_POWER

		config MYNEWT_VAL_BLE_MESH_LPN_ESTABLISHMENT
		    int "Perform the Friendship establishment using low power, with the help of a reduced scan duty cycle"
		    default 1

		    help 
				Perform the Friendship establishment using low power, with the help of a reduced scan duty cycle. The downside of this is that the node may miss out on messages intended for it until it has successfully set up Friendship with a Friend node.

		config MYNEWT_VAL_BLE_MESH_LPN_AUTO
		    int "Automatically enable LPN functionality once provisioned and start looking for Friend nodes"
		    default 1

		    help 
				Automatically enable LPN functionality once provisioned and start looking for Friend nodes. If this option is disabled LPN mode needs to be manually enabled by calling bt_mesh_lpn_set(true). node.

		config MYNEWT_VAL_BLE_MESH_LPN_AUTO_TIMEOUT
		    int "Time in seconds from the last received message, that the node will wait before starting to look for Friend nodes"
		    default 15

		    help 
				Time in seconds from the last received message, that the node will wait before starting to look for Friend nodes.

		config MYNEWT_VAL_BLE_MESH_LPN_RETRY_TIMEOUT
		    int "Time in seconds between Friend Requests, if a previous Friend Request did not receive any acceptable Friend Offers"
		    default 8

		    help 
				Time in seconds between Friend Requests, if a previous Friend Request did not receive any acceptable Friend Offers.

		config MYNEWT_VAL_BLE_MESH_LPN_RSSI_FACTOR
		    int "The contribution of the RSSI measured by the Friend node used in Friend Offer Delay calculations"
		    default 0

		    help 
				The contribution of the RSSI measured by the Friend node used in Friend Offer Delay calculations. 0 = 1, 1 = 1.5, 2 = 2, 3 = 2.5.

		config MYNEWT_VAL_BLE_MESH_LPN_RECV_WIN_FACTOR
		    int "The contribution of the supported Receive Window used in Friend Offer Delay calculations"
		    default 0

		    help 
				The contribution of the supported Receive Window used in Friend Offer Delay calculations. 0 = 1, 1 = 1.5, 2 = 2, 3 = 2.5.

		config MYNEWT_VAL_BLE_MESH_LPN_MIN_QUEUE_SIZE
		    int "The MinQueueSizeLog field is defined as log_2(N), where N is the minimum number of maximum size Lower Transport PDUs that the Friend node can store in its Friend Queue"
		    default 1

		    help 
				The MinQueueSizeLog field is defined as log_2(N), where N is the minimum number of maximum size Lower Transport PDUs that the Friend node can store in its Friend Queue. As an example, MinQueueSizeLog value 1 gives N = 2, and value 7 gives N = 128.

		config MYNEWT_VAL_BLE_MESH_LPN_RECV_DELAY
		    int "The ReceiveDelay is the time between the Low Power node sending a request and listening for a response"
		    default 100

		    help 
				The ReceiveDelay is the time between the Low Power node sending a request and listening for a response. This delay allows the Friend node time to prepare the response. The value is in units of milliseconds.

		config MYNEWT_VAL_BLE_MESH_LPN_POLL_TIMEOUT
		    int "PollTimeout timer is used to measure time between two consecutive requests sent by the Low Power node"
		    default 300

		    help 
				PollTimeout timer is used to measure time between two consecutive requests sent by the Low Power node. If no requests are received by the Friend node before the PollTimeout timer expires, then the friendship is considered terminated. The value is in units of 100 milliseconds, so e.g. a value of 300 means 30 seconds.

		config MYNEWT_VAL_BLE_MESH_LPN_INIT_POLL_TIMEOUT
		    int "The initial value of the PollTimeout timer when Friendship gets established for the first time"
		    default MYNEWT_VAL_BLE_MESH_LPN_POLL_TIMEOUT

		    help 
				The initial value of the PollTimeout timer when Friendship gets established for the first time. After this the timeout will gradually grow toward the actual PollTimeout, doubling in value for each iteration. The value is in units of 100 milliseconds, so e.g. a value of 300 means 3 seconds.

		config MYNEWT_VAL_BLE_MESH_LPN_SCAN_LATENCY
		    int "Latency in milliseconds that it takes to enable scanning"
		    default 10

		    help 
				Latency in milliseconds that it takes to enable scanning. This is in practice how much time in advance before the Receive Window that scanning is requested to be enabled.

		config MYNEWT_VAL_BLE_MESH_LPN_GROUPS
		    int "Maximum number of groups that the LPN can subscribe to."
		    default 10



        # config MYNEWT_VAL_BLE_MESH_FRIEND
        #    int "Enable this option to be able to act as a Friend Node."
        #    default 0
        config BLE_MESH_FRIEND
            bool "Enable this option to be able to act as a Friend Node."
            default n
        config MYNEWT_VAL_BLE_MESH_FRIEND
            int 
            default 0 if !BLE_MESH_FRIEND
            default 1 if BLE_MESH_FRIEND

		config MYNEWT_VAL_BLE_MESH_FRIEND_RECV_WIN
		    int "Receive Window in milliseconds supported by the Friend node."
		    default 255


		config MYNEWT_VAL_BLE_MESH_FRIEND_QUEUE_SIZE
		    int "Minimum number of buffers available to be stored for each local Friend Queue."
		    default 16


		config MYNEWT_VAL_BLE_MESH_FRIEND_SUB_LIST_SIZE
		    int "Size of the Subscription List that can be supported by a Friend node for a Low Power node."
		    default 3


		config MYNEWT_VAL_BLE_MESH_FRIEND_LPN_COUNT
		    int "Number of Low Power Nodes the Friend can have a Friendship with simultaneously."
		    default 2


		config MYNEWT_VAL_BLE_MESH_FRIEND_SEG_RX
		    int "Number of incomplete segment lists that we track for each LPN that we are Friends for"
		    default 1

		    help 
				Number of incomplete segment lists that we track for each LPN that we are Friends for. In other words, this determines how many elements we can simultaneously be receiving segmented messages from when the messages are going into the Friend queue.


        # config MYNEWT_VAL_BLE_MESH_CFG_CLI
        #    int "Enable support for the configuration client model."
        #    default 0
        config BLE_MESH_CFG_CLI
            bool "Enable support for the configuration client model."
			default y if BLE_MESH_SHELL
            default n
        config MYNEWT_VAL_BLE_MESH_CFG_CLI
            int 
            default 0 if !BLE_MESH_CFG_CLI
            default 1 if BLE_MESH_CFG_CLI


        # config MYNEWT_VAL_BLE_MESH_HEALTH_CLI
        #    int "Enable support for the health client model."
        #    default 0
        config BLE_MESH_HEALTH_CLI
            bool "Enable support for the health client model."
			default y if BLE_MESH_SHELL
            default n
        config MYNEWT_VAL_BLE_MESH_HEALTH_CLI
            int 
            default 0 if !BLE_MESH_HEALTH_CLI
            default 1 if BLE_MESH_HEALTH_CLI

		# config MYNEWT_VAL_BLE_MESH_SHELL
		#     int "Activate shell module that provides Bluetooth Mesh commands to the console."
		#     default 0
		config BLE_MESH_SHELL
		    bool "Activate shell module that provides Bluetooth Mesh commands to the console."
		    default n
		config MYNEWT_VAL_BLE_MESH_SHELL
            int 
            default 0 if !BLE_MESH_SHELL
            default 1 if BLE_MESH_SHELL



        # config MYNEWT_VAL_BLE_MESH_MODEL_EXTENSIONS
        #    int Enable support for the model extension concept, allowing the Access layer to know about Mesh model relationships.
        #    default 0
        config BLE_MESH_MODEL_EXTENSIONS
            bool "Enable support for the model extension concept, allowing the Access layer to know about Mesh model relationships"
            default n
            help
                Enable support for the model extension concept, allowing the Access layer to know about Mesh model relationships.
        config MYNEWT_VAL_BLE_MESH_MODEL_EXTENSIONS
            int 
            default 0 if !BLE_MESH_MODEL_EXTENSIONS
            default 1 if BLE_MESH_MODEL_EXTENSIONS

		# config MYNEWT_VAL_BLE_MESH_IV_UPDATE_TEST
		#     int "This option removes the 96 hour limit of the IV Update Procedure and lets the state be changed at any time"
		#     default 0
		#     help 
		# 		This option removes the 96 hour limit of the IV Update Procedure and lets the state be changed at any time.
		config BLE_MESH_IV_UPDATE_TEST
		    bool "This option removes the 96 hour limit of the IV Update Procedure and lets the state be changed at any time"
			default y if BLE_MESH_SHELL
		    default n
		    help 
				This option removes the 96 hour limit of the IV Update Procedure and lets the state be changed at any time.
		config MYNEWT_VAL_BLE_MESH_IV_UPDATE_TEST
            int 
            default 0 if !BLE_MESH_IV_UPDATE_TEST
            default 1 if BLE_MESH_IV_UPDATE_TEST

		config MYNEWT_VAL_BLE_MESH_TESTING
		    int "This option enables testing API."
		    default 0


		# config MYNEWT_VAL_BLE_MESH_DEV_UUID
		#     int "Device UUID"
		#     default ((uint8_t[16]){0x11, 0x22, 0})


		config MYNEWT_VAL_BLE_MESH_SHELL_MODELS
		    int "Include implementation of some demo models."
		    default 0


		config MYNEWT_VAL_BLE_MESH_OOB_OUTPUT_ACTIONS
		    hex "Supported Output OOB Actions BT_MESH_NO_OUTPUT=0, BT_MESH_BLINK=BIT(0) BT_MESH_BEEP=BIT(1) BT_MESH_VIBRATE=BIT(2) BT_MESH_DISPLAY_NUMBER=BIT(3) BT_MESH_DISPLAY_STRING=BIT(4)"
		    default 0x08


		config MYNEWT_VAL_BLE_MESH_OOB_OUTPUT_SIZE
		    int "Output OOB size"
		    default 4


		config MYNEWT_VAL_BLE_MESH_OOB_INPUT_ACTIONS
		    hex "Supported Input OOB Actions BT_MESH_NO_INPUT=0, BT_MESH_PUSH=BIT(0) BT_MESH_TWIST=BIT(1) BT_MESH_ENTER_NUMBER=BIT(2) BT_MESH_ENTER_STRING=BIT(3)"
		    default 0


		config MYNEWT_VAL_BLE_MESH_OOB_INPUT_SIZE
		    int "Input OOB size"
		    default 4


		config MYNEWT_VAL_BLE_MESH_SETTINGS
		    int "This option enables Mesh settings storage."
		    default 1


		config MYNEWT_VAL_BLE_MESH_STORE_TIMEOUT
		    int "This value defines in seconds how soon any pending changes are actually written into persistent storage (flash) after a change occurs"
		    default 2

		    help 
				This value defines in seconds how soon any pending changes are actually written into persistent storage (flash) after a change occurs.

		config MYNEWT_VAL_BLE_MESH_SEQ_STORE_RATE
		    int "This value defines how often the local sequence number gets updated in persistent storage (i"
		    default 128

		    help 
				This value defines how often the local sequence number gets updated in persistent storage (i.e. flash). E.g. a value of 100 means that the sequence number will be stored to flash on every 100th increment. If the node sends messages very frequently a higher value makes more sense, whereas if the node sends infrequently a value as low as 0 (update storage for every increment) can make sense. When the stack gets initialized it will add this number to the last stored one, so that it starts off with a value that's guaranteed to be larger than the last one used before power off.

		config MYNEWT_VAL_BLE_MESH_RPL_STORE_TIMEOUT
		    int "This value defines in seconds how soon the RPL gets written to persistent storage after a change occurs"
		    default 5

		    help 
				This value defines in seconds how soon the RPL gets written to persistent storage after a change occurs. If the node receives messages frequently it may make sense to have this set to a large value, whereas if the RPL gets updated infrequently a value as low as 0 (write immediately) may make sense. Note that if the node operates a security sensitive use case, and there's a risk of sudden power loss, it may be a security vulnerability to set this value to anything else than 0 (a power loss before writing to storage exposes the node to potential message replay attacks).

		config MYNEWT_VAL_BLE_MESH_DEVICE_NAME
		    string "This value defines BLE Mesh device/node name."
		    default "nimble-mesh-node"

		config MYNEWT_VAL_BLE_MESH_SYSINIT_STAGE
		    int "Primary sysinit stage for BLE mesh functionality."
		    default 500


		config MYNEWT_VAL_BLE_MESH_SYSINIT_STAGE_SHELL
		    int "Secondary sysinit stage for BLE mesh functionality."
		    default 1000


		config MYNEWT_VAL_BLE_MESH_LOG_MOD
		    int "Numeric module ID to use for BLE Mesh log messages."
		    default 9


		config MYNEWT_VAL_BLE_MESH_LOG_LVL
		    int "Minimum level for the BLE Mesh log."
		    default 1


		config MYNEWT_VAL_BLE_MESH_ACCESS_LOG_MOD
		    int "Numeric module ID to use for BLE Mesh Access-related log messages."
		    default 10


		config MYNEWT_VAL_BLE_MESH_ACCESS_LOG_LVL
		    int "Minimum level for the BLE Mesh Access-related log."
		    default 1


		config MYNEWT_VAL_BLE_MESH_ADV_LOG_MOD
		    int "Numeric module ID to use for BLE Mesh advertising log messages."
		    default 11


		config MYNEWT_VAL_BLE_MESH_ADV_LOG_LVL
		    int "Minimum level for the BLE Mesh log."
		    default 1


		config MYNEWT_VAL_BLE_MESH_BEACON_LOG_MOD
		    int "Numeric module ID to use for BLE Mesh Beacon-related log messages."
		    default 12


		config MYNEWT_VAL_BLE_MESH_BEACON_LOG_LVL
		    int "Minimum level for the BLE Mesh Beacon-related log."
		    default 1


		config MYNEWT_VAL_BLE_MESH_CRYPTO_LOG_MOD
		    int "Numeric module ID to use for BLE Mesh cryptographic log messages."
		    default 13


		config MYNEWT_VAL_BLE_MESH_CRYPTO_LOG_LVL
		    int "Minimum level for the BLE Mesh cryptographic log."
		    default 1


		config MYNEWT_VAL_BLE_MESH_FRIEND_LOG_MOD
		    int "Numeric module ID to use for BLE Mesh Friend log messages."
		    default 14


		config MYNEWT_VAL_BLE_MESH_FRIEND_LOG_LVL
		    int "Minimum level for the BLE Mesh Friend log."
		    default 1


		config MYNEWT_VAL_BLE_MESH_LOW_POWER_LOG_MOD
		    int "Numeric module ID to use for BLE Mesh Low Power log messages."
		    default 15


		config MYNEWT_VAL_BLE_MESH_LOW_POWER_LOG_LVL
		    int "Minimum level for the BLE Mesh Low Power log."
		    default 1


		config MYNEWT_VAL_BLE_MESH_MODEL_LOG_MOD
		    int "Numeric module ID to use for BLE Mesh Foundation Models log messages."
		    default 16


		config MYNEWT_VAL_BLE_MESH_MODEL_LOG_LVL
		    int "Minimum level for the BLE Mesh Foundation Models log."
		    default 1


		config MYNEWT_VAL_BLE_MESH_NET_LOG_MOD
		    int "Numeric module ID to use for BLE Mesh Network layer log messages."
		    default 17


		config MYNEWT_VAL_BLE_MESH_NET_LOG_LVL
		    int "Minimum level for the BLE Mesh Network layer log."
		    default 1


		config MYNEWT_VAL_BLE_MESH_PROV_LOG_MOD
		    int "Numeric module ID to use for BLE Mesh Provisioning log messages."
		    default 18


		config MYNEWT_VAL_BLE_MESH_PROV_LOG_LVL
		    int "Minimum level for the BLE Mesh Provisioning log."
		    default 1


		config MYNEWT_VAL_BLE_MESH_PROXY_LOG_MOD
		    int "Numeric module ID to use for BLE Mesh Proxy protocol log messages."
		    default 19


		config MYNEWT_VAL_BLE_MESH_PROXY_LOG_LVL
		    int "Minimum level for the BLE Mesh Proxy protocol log."
		    default 1


		config MYNEWT_VAL_BLE_MESH_SETTINGS_LOG_MOD
		    int "Numeric module ID to use for BLE Mesh persistent settings log messages."
		    default 20


		config MYNEWT_VAL_BLE_MESH_SETTINGS_LOG_LVL
		    int "Minimum level for the BLE Mesh persistent settings log."
		    default 1


		config MYNEWT_VAL_BLE_MESH_TRANS_LOG_MOD
		    int "Numeric module ID to use for BLE Mesh Transport Layer log messages."
		    default 21


		config MYNEWT_VAL_BLE_MESH_TRANS_LOG_LVL
		    int "Minimum level for the BLE Mesh Transport Layer log."
		    default 1

    endif