menu "Transport"
choice
    prompt "HCI transport Select"
    default BLE_USING_RAM
    help
        Selects HCI transport to be included in build. This has virtually the same effect as including package dependency manually, but it allows to easily override HCI transport package in application or target settings.

    config BLE_USING_RAM
        bool "ram"

    config BLE_USING_UART
        bool "uart"

    config BLE_USING_SOCKET
        bool "socket"

    config BLE_USING_USB
        bool "usb"

endchoice
    if BLE_USING_RAM
        source "$OS_ROOT/components/ble/mynewt-nimble/nimble/transport/ram/Kconfig"
    endif

    if BLE_USING_UART
        source "$OS_ROOT/components/ble/mynewt-nimble/nimble/transport/uart/Kconfig"
    endif

    if BLE_USING_SOCKET
        source "$OS_ROOT/components/ble/mynewt-nimble/nimble/transport/socket/Kconfig"
    endif

    if BLE_USING_USB
        source "$OS_ROOT/components/ble/mynewt-nimble/nimble/transport/usb/Kconfig"
    endif

endmenu