config MYNEWT_VAL_
    int ""
    default 

config MYNEWT_VAL_BLE_HCI_EMSPI
    int "Indicates that the emspi host HCI transport is present."
    default 1


config MYNEWT_VAL_    restrictions
    int "Indicates that the emspi host HCI transport is present."
    default 1


config MYNEWT_VAL_BLE_HCI_EVT_HI_BUF_COUNT
    int "Number of high-priority event buffers."
    default  2


config MYNEWT_VAL_BLE_HCI_EVT_LO_BUF_COUNT
    int "Number of low-priority event buffers."
    default  8


config MYNEWT_VAL_BLE_HCI_EVT_BUF_SIZE
    int "Size of each event buffer, in bytes."
    default  70


config MYNEWT_VAL_BLE_ACL_BUF_COUNT
    int "The number of ACL data buffers"
    default 4


config MYNEWT_VAL_BLE_ACL_BUF_SIZE
    int "This is the maximum size of the data portion of HCI ACL datapackets. It does not include the HCI data header (of 4 bytes)."
    default 255


config MYNEWT_VAL_BLE_HCI_ACL_OUT_COUNT
    int "This count is used in creating a pool of elements used by thecode to enqueue various elements. In the case of the controlleronly HCI, this number should be equal to the number of mbufs inthe msys pool. For host only, it is really dependent on thenumber of ACL buffers that the controller tells the host ithas."
    default 12


config MYNEWT_VAL_BLE_HCI_EMSPI_SPI_NUM
    int "This count is used in creating a pool of elements used by thecode to enqueue various elements. In the case of the controlleronly HCI, this number should be equal to the number of mbufs inthe msys pool. For host only, it is really dependent on thenumber of ACL buffers that the controller tells the host ithas."
    default 5


config MYNEWT_VAL_BLE_HCI_EMSPI_BAUD
    int "This count is used in creating a pool of elements used by thecode to enqueue various elements. In the case of the controlleronly HCI, this number should be equal to the number of mbufs inthe msys pool. For host only, it is really dependent on thenumber of ACL buffers that the controller tells the host ithas."
    default 8000000


config MYNEWT_VAL_BLE_HCI_EMSPI_RESET_PIN
    int "This count is used in creating a pool of elements used by thecode to enqueue various elements. In the case of the controlleronly HCI, this number should be equal to the number of mbufs inthe msys pool. For host only, it is really dependent on thenumber of ACL buffers that the controller tells the host ithas."
    default 42


config MYNEWT_VAL_BLE_HCI_EMSPI_SS_PIN
    int "This count is used in creating a pool of elements used by thecode to enqueue various elements. In the case of the controlleronly HCI, this number should be equal to the number of mbufs inthe msys pool. For host only, it is really dependent on thenumber of ACL buffers that the controller tells the host ithas."
    default 45


config MYNEWT_VAL_BLE_HCI_EMSPI_RDY_PIN
    int "The GPIO pin that the EM controller uses to indicate data ready."
    default 26


config MYNEWT_VAL_BLE_HCI_EMSPI_PRIO
    int "The GPIO pin that the EM controller uses to indicate data ready."
    default 5


config MYNEWT_VAL_BLE_HCI_EMSPI_STACK_SIZE
    int "The size of the emspi task (units: 4-byte words)."
    default 256