menu "ram"
		config MYNEWT_VAL_BLE_HCI_EVT_HI_BUF_COUNT
		    int "Number of high-priority event buffers."
		    default  2


		config MYNEWT_VAL_BLE_HCI_EVT_LO_BUF_COUNT
		    int "Number of low-priority event buffers."
		    default  8


		config MYNEWT_VAL_BLE_HCI_EVT_BUF_SIZE
		    int "Size of each event buffer, in bytes."
			default  257 if BLE_EXT_ADV
		    default  70


		config MYNEWT_VAL_BLE_ACL_BUF_COUNT
		    int "The number of ACL data buffers"
		    default 4


		config MYNEWT_VAL_BLE_ACL_BUF_SIZE
		    int "This is the maximum size of the data portion of HCI ACL data packets"
		    default 255

		    help 
				This is the maximum size of the data portion of HCI ACL data packets. It does not include the HCI data header (of 4 bytes).

		config MYNEWT_VAL_BLE_TRANS_RAM_SYSINIT_STAGE
		    int "Sysinit stage for the RAM BLE transport."
		    default 100
endmenu