menu "socket"
		config MYNEWT_VAL_BLE_HCI_EVT_BUF_SIZE
		    int "The size of the allocated event buffers"
			default 257 if BLE_EXT_ADV
		    default 70


		config MYNEWT_VAL_BLE_HCI_EVT_HI_BUF_COUNT
		    int "The number of high priority event buffers"
		    default 8


		config MYNEWT_VAL_BLE_HCI_EVT_LO_BUF_COUNT
		    int "The number of low priority event buffers"
		    default 8


		config MYNEWT_VAL_BLE_ACL_BUF_COUNT
		    int "The number of ACL data buffers"
		    default 24


		config MYNEWT_VAL_BLE_ACL_BUF_SIZE
		    int "This is the maximum size of the data portion of HCI ACL data packets"
		    default 255

		    help 
				This is the maximum size of the data portion of HCI ACL data packets. It does not include the HCI data header (of 4 bytes).

		config MYNEWT_VAL_BLE_HCI_ACL_OUT_COUNT
		    int "This count is used in creating a pool of elements used by the code to enqueue various elements"
		    default 12

		    help 
				This count is used in creating a pool of elements used by the code to enqueue various elements. In the case of the controller only HCI, this number should be equal to the number of mbufs in the msys pool. For host only, it is really dependent on the number of ACL buffers that the controller tells the host it has.

		config MYNEWT_VAL_BLE_SOCK_USE_TCP
		    int "Use TCP socket, connects to BLE_SOCK_TCP_PORT"
		    default 1


		config MYNEWT_VAL_BLE_SOCK_TCP_PORT
		    int "ipv4 tcp port to connect to"
		    default 14433


		config MYNEWT_VAL_BLE_SOCK_USE_LINUX_BLUE
		    int "Use Linux bluetooth raw socket"
		    default 0


		config MYNEWT_VAL_BLE_SOCK_LINUX_DEV
		    int "linux kernel device"
		    default 0


		config MYNEWT_VAL_BLE_SOCK_TASK_PRIO
		    int "Priority of the HCI socket task."
		    default 9


		config MYNEWT_VAL_BLE_SOCK_STACK_SIZE
		    int "Size of the HCI socket stack (units=words)."
		    default 80


		config MYNEWT_VAL_BLE_SOCK_CLI_SYSINIT_STAGE
		    int "Sysinit stage for the socket BLE transport."
		    default 500

endmenu