menu "BC28 Config" 

    config BC28_AUTO_CREATE
        bool "Enable BC28 Module Object Auto Create"
        select MOLINK_USING_AUTO_CREATE
        default n

    if BC28_AUTO_CREATE

        config BC28_DEVICE_NAME
            string "BC28 Interface Device Name"
            default "uart2"

        config BC28_DEVICE_RATE
            int "BC28 Interface Device Rate"
            default 9600

        config BC28_RECV_BUFF_LEN
            int "The maximum length of AT command data accepted"
            default 512

    endif

    config BC28_USING_GENERAL_OPS
        bool "Enable BC28 Module General Operates"
        select MOLINK_USING_GENERAL_OPS
        default y
    
    config BC28_USING_NETSERV_OPS
        bool "Enable BC28 Module Network Service Operates"
        select MOLINK_USING_NETSERV_OPS
        default y

    config BC28_USING_PING_OPS
        bool "Enable BC28 Module Ping Operates"
        select MOLINK_USING_NETSERV_OPS
        select MOLINK_USING_PING_OPS
        default y

    config BC28_USING_IFCONFIG_OPS
        bool "Enable BC28 Module Ifconfig Operates"
        select MOLINK_USING_IFCONFIG_OPS
        select BC28_USING_GENERAL_OPS
        select BC28_USING_NETSERV_OPS
        default y

    config BC28_USING_NETCONN_OPS
        bool "Enable BC28 Module Network TCP/IP Operates"
        select MOLINK_USING_NETCONN_OPS
        select BC28_USING_NETSERV_OPS
        default y

    config BC28_USING_SOCKETS_OPS
        bool "Enable BC28 Module BSD Socket Operates"
        select BC28_USING_NETCONN_OPS
        select MOLINK_USING_SOCKETS_OPS
        default n

    config BC28_USING_ONENET_NB_OPS
        bool "Enable BC28 Module Onenet Nb Operates"
        select MOLINK_USING_ONENET_NB_OPS
        default y

        if BC28_USING_ONENET_NB_OPS

        config BC28_RESP_BUFF_SIZE
            int "The OneNET AT Parser stack size"
            default 128

        config BC28_URC_MANAGER_TASK_PRIORITY
            hex "The URC manager task priority"
            default 0x10

        config BC28_URC_MANAGER_STACK_SIZE
            int "The URC manager task stack size"
            default 2048
    endif

endmenu