menu "BC95 Config" 

    config BC95_AUTO_CREATE
        bool "Enable BC95 Module Object Auto Create"
        select MOLINK_USING_AUTO_CREATE
        default n

    if BC95_AUTO_CREATE

        config BC95_DEVICE_NAME
            string "BC95 Interface Device Name"
            default "uart2"

        config BC95_DEVICE_RATE
            int "BC95 Interface Device Rate"
            default 9600

        config BC95_RECV_BUFF_LEN
            int "The maximum length of AT command data accepted"
            default 512

    endif

    config BC95_USING_GENERAL_OPS
        bool "Enable BC95 Module General Operates"
        select MOLINK_USING_GENERAL_OPS
        default y
    
    config BC95_USING_NETSERV_OPS
        bool "Enable BC95 Module Network Service Operates"
        select MOLINK_USING_NETSERV_OPS
        default y

    config BC95_USING_PING_OPS
        bool "Enable BC95 Module Ping Operates"
        select MOLINK_USING_NETSERV_OPS
        select MOLINK_USING_PING_OPS
        default y

    config BC95_USING_IFCONFIG_OPS
        bool "Enable BC95 Module Ifconfig Operates"
        select MOLINK_USING_IFCONFIG_OPS
        select BC95_USING_GENERAL_OPS
        select BC95_USING_NETSERV_OPS
        default y

    config BC95_USING_NETCONN_OPS
        bool "Enable BC95 Module Network TCP/IP Operates"
        select MOLINK_USING_NETCONN_OPS
        select BC95_USING_NETSERV_OPS
        default y

    config BC95_USING_SOCKETS_OPS
        bool "Enable BC95 Module BSD Socket Operates"
        select BC95_USING_NETCONN_OPS
        select MOLINK_USING_SOCKETS_OPS
        default n

    config BC95_USING_ONENET_NB_OPS
        bool "Enable BC95 Module Onenet Nb Operates"
        select MOLINK_USING_ONENET_NB_OPS
        default y

    if BC95_USING_ONENET_NB_OPS

        config BC95_RESP_BUFF_SIZE
            int "The OneNET AT Parser stack size"
            default 128

        config BC95_URC_MANAGER_TASK_PRIORITY
            hex "The URC manager task priority"
            default 0x10

        config BC95_URC_MANAGER_STACK_SIZE
            int "The URC manager task stack size"
            default 2048

    endif

endmenu