menu "ESP8266 Config" 

    config ESP8266_AUTO_CREATE
        bool "Enable ESP8266 Module Object Auto Create"
        default n

    if ESP8266_AUTO_CREATE

        config ESP8266_DEVICE_NAME
            string "ESP8266 Interface Device Name"
            default "uart2"

        config ESP8266_DEVICE_RATE
            int "ESP8266 Interface Device Rate"
            default 115200

        config ESP8266_RECV_BUFF_LEN
            int "The maximum length of AT command data accepted"
            default 512

        config ESP8266_AUTO_CONNECT_AP
            bool "Enable ESP8266 Module Auto Connect"
            select ESP8266_USING_WIFI_OPS
            default y
    endif

    config ESP8266_CONNECT_SSID
        string "ESP8266 Connect AP SSID"
        default "ssid"

    config ESP8266_CONNECT_PASSWORD
        string "ESP8266 Connect AP Password"
        default "password"

    config ESP8266_USING_GENERAL_OPS
        bool "Enable ESP8266 Module General Operates"
        select MOLINK_USING_GENERAL_OPS
        default y

    config ESP8266_USING_WIFI_OPS
        bool "Enable ESP8266 Module WiFi Operates"
        select MOLINK_USING_WIFI_OPS
        default y

    config ESP8266_USING_PING_OPS
        bool "Enable ESP8266 Module Ping Operates"
        select MOLINK_USING_PING_OPS
        default y

    config ESP8266_USING_IFCONFIG_OPS
        bool "Enable ESP8266 Module Ifconfig Operates"
        select MOLINK_USING_IFCONFIG_OPS
        select ESP8266_USING_WIFI_OPS
        default y

    config ESP8266_USING_NETCONN_OPS
        bool "Enable ESP8266 Module Network TCP/IP Operates"
        select OS_USING_EVENT
        select MOLINK_USING_NETCONN_OPS
        default y

    config ESP8266_USING_SOCKETS_OPS
        bool "Enable ESP8266 Module BSD Socket Operates"
        select ESP8266_USING_NETCONN_OPS
        select MOLINK_USING_SOCKETS_OPS
        default n

    config ESP8266_USING_HW_CONTROL
        bool "Enable ESP8266 Module Hardware Control Operates"
        select OS_USING_PIN
        default n

        if ESP8266_USING_HW_CONTROL
            config ESP8266_RST_PIN_NUM
                int "The ESP8266 Module Reset Pin Number"
                help 
                    This can be calculated using GET_PIN(PORTx, PIN)
                default -1

        endif
endmenu