menu "GM190 Config" 

    config GM190_AUTO_CREATE
        bool "Enable GM190 Module Object Auto Create"
        default n

    if GM190_AUTO_CREATE

        config GM190_DEVICE_NAME
            string "GM190 Interface Device Name"
            default "uart2"

        config GM190_DEVICE_RATE
            int "GM190 Interface Device Rate"
            default 115200

        config GM190_RECV_BUFF_LEN
            int "The maximum length of AT command data accepted"
            default 512

    endif

    config GM190_USING_GENERAL_OPS
        bool "Enable GM190 Module General Operates"
        select MOLINK_USING_GENERAL_OPS
        default y
		
    config GM190_USING_NETSERV_OPS
        bool "Enable GM190 Module Network Service Operates"
        select MOLINK_USING_NETSERV_OPS
        default y

    config GM190_USING_IFCONFIG_OPS
        bool "Enable GM190 Module Ifconfig Operates"
        select MOLINK_USING_IFCONFIG_OPS
        select GM190_USING_GENERAL_OPS
        select GM190_USING_NETSERV_OPS
        default y
		
    config GM190_USING_NETCONN_OPS
        bool "Enable GM190 Module Network TCP/IP Operates"
        select MOLINK_USING_NETCONN_OPS
        default y

    config GM190_USING_SOCKETS_OPS
        bool "Enable GM190 Module BSD Socket Operates"
        select GM190_USING_NETCONN_OPS
        select MOLINK_USING_SOCKETS_OPS
        default n

endmenu