menu "M5311 Config" 

    config M5311_AUTO_CREATE
        bool "Enable M5311 Module Object Auto Create"
        default n

    if M5311_AUTO_CREATE

        config M5311_DEVICE_NAME
            string "M5311 Interface Device Name"
            default "uart2"

        config M5311_DEVICE_RATE
            int "M5311 Interface Device Rate"
            default 115200

        config M5311_RECV_BUFF_LEN
            int "The maximum length of AT command data accepted"
            default 512

    endif

    config M5311_USING_GENERAL_OPS
        bool "Enable M5311 Module General Operates"
        select MOLINK_USING_GENERAL_OPS
        default y
    
    config M5311_USING_NETSERV_OPS
        bool "Enable M5311 Module Network Service Operates"
        select MOLINK_USING_NETSERV_OPS
        default y

    config M5311_USING_PING_OPS
        bool "Enable M5311 Module Ping Operates"
        select MOLINK_USING_PING_OPS
        default y

    config M5311_USING_IFCONFIG_OPS
        bool "Enable M5311 Module Ifconfig Operates"
        select MOLINK_USING_IFCONFIG_OPS
        select M5311_USING_GENERAL_OPS
        select M5311_USING_NETSERV_OPS
        default y

    config M5311_USING_NETCONN_OPS
        bool "Enable M5311 Module Network TCP/IP Operates"
        select MOLINK_USING_NETCONN_OPS
        default y

    config M5311_USING_SOCKETS_OPS
        bool "Enable M5311 Module BSD Socket Operates"
        select M5311_USING_NETCONN_OPS
        select MOLINK_USING_SOCKETS_OPS
        default n

    config M5311_USING_ONENET_NB_OPS
        bool "Enable M5311 Module Onenet Nb Operates"
        select MOLINK_USING_ONENET_NB_OPS
        default y

endmenu