menu "ML302 Config" 

    config ML302_AUTO_CREATE
        bool "Enable ML302 Module Object Auto Create"
        default n

    if ML302_AUTO_CREATE

        config ML302_DEVICE_NAME
            string "ML302 Interface Device Name"
            default "uart2"

        config ML302_DEVICE_RATE
            int "ML302 Interface Device Rate"
            default 115200

        config ML302_RECV_BUFF_LEN
            int "The maximum length of AT command data accepted"
            default 512

    endif

    config ML302_USING_GENERAL_OPS
        bool "Enable ML302 Module General Operates"
        select MOLINK_USING_GENERAL_OPS
        default y
    
    config ML302_USING_NETSERV_OPS
        bool "Enable ML302 Module Network Service Operates"
        select MOLINK_USING_NETSERV_OPS
        default y

    config ML302_USING_PING_OPS
        bool "Enable ML302 Module Ping Operates"
        select MOLINK_USING_PING_OPS
        default y

    config ML302_USING_IFCONFIG_OPS
        bool "Enable ML302 Module Ifconfig Operates"
        select MOLINK_USING_IFCONFIG_OPS
        select ML302_USING_GENERAL_OPS
        select ML302_USING_NETSERV_OPS
        default y

    config ML302_USING_NETCONN_OPS
        bool "Enable ML302 Module Network TCP/IP Operates"
        select MOLINK_USING_NETCONN_OPS
        default y

    config ML302_USING_SOCKETS_OPS
        bool "Enable ML302 Module BSD Socket Operates"
        select ML302_USING_NETCONN_OPS
        select MOLINK_USING_SOCKETS_OPS
        default n

endmenu