menu "Websocket Client"


config WEBSOCKET_CLIENT_TASK_MAX_INSTANCE
	int "The maximum number of websocket client instances"
	range 1 9
	default 1	
	
config WEBSOCKET_CLIENT_TASK_STACKSIZE
	int "The stack size of task"
	default 2048
	
config WEBSOCKET_CLIENT_TASK_PRIORITY
	int "The priority level value of task"	
	default 5   if OS_TASK_PRIORITY_8
	default 13  if OS_TASK_PRIORITY_32
	default 64 if OS_TASK_PRIORITY_256
	
config WEBSOCKET_CLIENT_TASK_TICK
	int "The tick of task"
	default 5
	
config WEBSOCKET_CLIENT_MAX_BUFF_DEP
	int "The maximum number of send & rece buffer depth"
	default 1452

config WEBSOCKET_CLIENT_EXAMPLE
    bool "Enable Websocket Client example"
    default n
	
endmenu