menu "Tools"

config NET_USING_TOOLS
    bool "Enable AT module network debug functions"
    default n
    select NET_USING_IP
    select OS_USING_SHELL

    if NET_USING_TOOLS

        config MODULE_USING_IFCONFIG
            bool "Enable module ifconfig features"
            depends on MOLINK_USING_IFCONFIG_OPS
            default y

        config MODULE_USING_PING
            depends on MOLINK_USING_PING_OPS && MOLINK_USING_IFCONFIG_OPS
            bool "Enable module ping features"
            default y

        if MODULE_USING_PING
            config MO_PING_MAX_TIMES_CONFIG
            int "The maximum times of module ping cmd config"
            default 50
        endif 

        config MODULE_USING_SOCKETSTAT
            depends on MOLINK_USING_SOCKETS_OPS
            bool "Enable module socket stat features"
            default y

    endif

endmenu