menu "Graphic"
    config OS_USING_GRAPHIC
        bool "Using graphic devices"
        default n

    if OS_USING_GRAPHIC
        config OS_GRAPHIC_WIDTH
            int "Graphic width"
            default 320

        config OS_GRAPHIC_HEIGHT
            int "Graphic height"
            default 240
    
        config OS_USING_DSI
            bool "Use DSI"
            default n
            
            if OS_USING_DSI
                config OS_USING_DSI_RST
                    int "dsi rst io"
                    default 159
            endif
            
        config BSP_USING_OTM8009A
            bool "Use otm8009a"
            default n
            
            if OS_USING_DSI && BSP_USING_OTM8009A
                config BSP_OTM8009A_DSI_CHANNEL
                    int "otm8009a DSI channel id"
                    default 0
            endif

        menuconfig BSP_USING_ILI9341
            bool "Enable ili9341"
            default n

            if BSP_USING_ILI9341
                config BSP_ILI9341_SPI_BUS_NAME
                    string "ili9341 spi bus name"
                    default "spi5"

                config BSP_ILI9341_SPI_CS
                    int "ili9341 spi cs io"
                    default 34

                config BSP_ILI9341_WRX
                    int "ili9341 wrx io"
                    default 61
            endif

        menuconfig OS_USING_ST7789VW
            bool "Use st7789vw"
            select OS_USING_SPI
            select BSP_USING_SPI
            default n

            if OS_USING_ST7789VW
                config OS_ST7789VW_SPI_BUS_NAME
                    string "st7789vw spi bus name"
                    default "spi1"

                config OS_ST7789VW_SPI_BUS_MODE
                    int "st7789vw spi bus mode"
                    default 0

                config OS_ST7789VW_SPI_CS_PIN
                    int "st7789vw spi cs pin"
                    default 62

                config OS_ST7789VW_PWR_PIN
                    int "st7789vw power pin"
                    default 4

                config OS_ST7789VW_PWR_PIN_ACTIVE
                    int "st7789vw power pin active level"
                    default 1

                config OS_ST7789VW_DC_PIN
                    int "st7789vw dc pin"
                    default 59

                config OS_ST7789VW_RES_PIN
                    int "st7789vw reset pin"
                    default 6
            endif
    endif

endmenu