menu "Infrared"
    config OS_USING_INFRARED
        bool "Using infrared device drivers"
        select OS_USING_TIMER_DRIVER
        select OS_USING_CLOCKSOURCE
        default n

    if OS_USING_INFRARED    
        menuconfig BSP_USING_RMT_CTL_ATK_TX
            bool "Enable atk remote control tx"
            default n

            if BSP_USING_RMT_CTL_ATK_TX
                config BSP_USING_RMT_CTL_ATK_TX_PIN
                    int "tx pin"
                    default 16
            endif
            
        menuconfig BSP_USING_RMT_CTL_ATK_RX
            bool "Enable atk remote control rx"
            default n

            if BSP_USING_RMT_CTL_ATK_RX
                config BSP_USING_RMT_CTL_ATK_RX_PIN
                    int "rx pin"
                    default 17
            endif
    endif

endmenu