menu "SDIO"
config OS_USING_SDIO
    bool "Using SD/MMC device drivers"
    default n

    if OS_USING_SDIO
        config OS_SDIO_STACK_SIZE
            int "The stack size for sdio irq thread"
            default 512

        config OS_SDIO_TASK_PRIORITY
            int "The priority level value of sdio irq thread"
            default 15

        config OS_MMCSD_STACK_SIZE
            int "The stack size for mmcsd thread"
            default 1024

        config OS_MMCSD_TASK_PREORITY
            int "The priority level value of mmcsd thread"
            default 22

        config OS_MMCSD_MAX_PARTITION
            int "mmcsd max partition"
            default 16
        config OS_SDIO_DEBUG
            bool "Enable SDIO debug log output"
        default n
    endif
endmenu