from build_tools import *
import osconfig

pwd = PresentDir()
src = ['spi_core.c', 'spi_dev.c']
CPPPATH = [pwd]
LOCAL_CCFLAGS = ''

if IsDefined('OS_USING_QSPI'):
    src += ['qspi_core.c']

src_device = []

if IsDefined('OS_USING_SPI_WIFI'):
    src_device += ['spi_wifi_rw009.c']

if IsDefined('BSP_USING_ENC28J60'):
    src_device += ['enc28j60.c']

if IsDefined('OS_USING_SPI_MSD'):
    src_device += ['spi_msd.c']
    src_device += ['spi_tfcard.c']
    
if IsDefined('OS_SFUD_USING_SPI'):
    src_device += ['flash/flash_spi.c']

if IsDefined('BSP_USING_AT45DBXX'):
    src_device += ['spi_flash_at45dbxx.c']
    
if IsDefined('OS_SFUD_USING_QSPI'):
    src += Glob('flash/flash_qspi.c')

if IsDefined('OS_USING_FAL') and (IsDefined('OS_SFUD_USING_SPI') or IsDefined('OS_SFUD_USING_QSPI')):
    src += Glob('flash/fal_flash_sfud_port.c')

if IsDefined('OS_USING_SFUD'):
    src_device += ['spi_flash_sfud.c', 'sfud/src/sfud.c']
    CPPPATH += [pwd + '/sfud/inc']
    if IsDefined('OS_SFUD_USING_SFDP'):
        src_device += ['sfud/src/sfud_sfdp.c']
        
src += src_device

group = AddCodeGroup('drivers', src, depend = ['OS_USING_SPI'], CPPPATH = CPPPATH, LOCAL_CCFLAGS = LOCAL_CCFLAGS)

Return('group')