menu "Touch"
    config OS_USING_TOUCH
    bool "Using Touch device drivers"
    default n

    if OS_USING_TOUCH
        config OS_TOUCH_X_SWAP
            bool "x coordinate swap"
            default n

        config OS_TOUCH_Y_SWAP
            bool "y coordinate swap"
            default n

        menuconfig OS_USING_GT9147
            bool "Enable gt9147"
            select OS_USING_I2C
            select BSP_USING_I2C
            default n

            if OS_USING_GT9147
                config OS_GT9147_I2C_BUS_NAME
                    string "gt9147 i2c bus name"
                    default "i2c1"

                config OS_GT9147_I2C_ADDR_HIGH
                    hex "gt9147 i2c addr high(7bit)"
                    default 0x5d

                config OS_GT9147_I2C_ADDR_LOW
                    hex "gt9147 i2c addr low"
                    default 0x14

                config OS_GT9147_RST_PIN
                    int "gt9147 rst pin"
                    default 61

                config OS_GT9147_IRQ_PIN
                    int "gt9147 irq pin"
                    default 63
            endif

        menuconfig OS_USING_FT6X06
            bool "Enable ft6x06"
            select OS_USING_I2C
            select BSP_USING_I2C
            default n

            if OS_USING_FT6X06
                config OS_FT6X060_I2C_BUS_NAME
                    string "ft6x06 i2c bus name"
                    default "i2c2"

                config OS_FT6X06_I2C_ADDR
                    hex "ft6x06 i2c addr(7bit)"
                    default 0x2a
            endif

        menuconfig OS_USING_STMPE811
            bool "Enable stmpe811"
            select OS_USING_I2C
            select BSP_USING_I2C
            default n

            if OS_USING_STMPE811
                config OS_STMPE811_I2C_BUS_NAME
                    string "stmpe811 i2c bus name"
                    default "i2c3"

                config OS_STMPE811_I2C_ADDR
                    hex "stmpe811 i2c addr(7bit)"
                    default 0x41
            endif
    endif
endmenu