menu "USB"
    config OS_USING_USB_DEVICE
        bool "Using USB device"
        default n
        if OS_USING_USB_DEVICE || OS_USING_USB_HOST
            config OS_USBD_TASK_STACK_SZ
                int "usb task stack size"
                default 4096
        endif
        if OS_USING_USB_DEVICE
            config USB_VENDOR_ID
                hex "USB Vendor ID"
                default 0x0FFE
            config USB_PRODUCT_ID
                hex "USB Product ID"
                default 0x0001

            config OS_USB_DEVICE_COMPOSITE
                bool "Enable composite device"
                default n
                choice
                    prompt "Device type"
                    default _OS_USB_DEVICE_NONE
                    depends on !OS_USB_DEVICE_COMPOSITE
                        config _OS_USB_DEVICE_NONE
                            bool "Using custom class by register interface"
                            select OS_USB_DEVICE_NONE
                        config _OS_USB_DEVICE_CDC
                            bool "Enable to use device as CDC device"
                            select OS_USB_DEVICE_CDC
                        config _OS_USB_DEVICE_MSTORAGE
                            bool "Enable to use device as Mass Storage device"
                            select OS_USB_DEVICE_MSTORAGE
                        config _OS_USB_DEVICE_HID
                            bool "Enable to use device as HID device"
                            select OS_USB_DEVICE_HID
                        config _OS_USB_DEVICE_RNDIS
                            bool "Enable to use device as rndis device"
                            select OS_USB_DEVICE_RNDIS
                            depends on NET_USING_LWIP
                        config _OS_USB_DEVICE_ECM
                            bool "Enable to use device as ecm device"
                            select OS_USB_DEVICE_ECM
                            depends on NET_USING_LWIP
                        config _OS_USB_DEVICE_WINUSB
                            bool "Enable to use device as winusb device"
                            select OS_USB_DEVICE_WINUSB
                        config _OS_USB_DEVICE_AUDIO
                            bool "Enable to use device as audio device"
                            select OS_USB_DEVICE_AUDIO
                endchoice

                    config OS_USB_DEVICE_CDC
                        bool "Enable to use device as CDC device"
                        default n
                    config OS_USB_DEVICE_NONE
                        bool
                        default y
                    config OS_USB_DEVICE_MSTORAGE
                        bool "Enable to use device as Mass Storage device"
                        default n
                    config OS_USB_DEVICE_HID
                        bool "Enable to use device as HID device"
                        default n
                    config OS_USB_DEVICE_RNDIS
                        bool "Enable to use device as rndis device"
                        default n
                        depends on NET_USING_LWIP
                    config OS_USB_DEVICE_ECM
                        bool "Enable to use device as ecm device"
                        default n
                        depends on NET_USING_LWIP
                    config OS_USB_DEVICE_WINUSB
                        bool "Enable to use device as winusb device"
                        default n
                    config OS_USB_DEVICE_AUDIO
                        bool "Enable to use device as audio device"
                        default n

                if OS_USB_DEVICE_CDC
                    config OS_VCOM_TASK_STK_SIZE
                        int "virtual com task stack size"
                        default 512
                    config OS_VCOM_TX_USE_DMA
                        bool "Enable to use dma for vcom tx"
                        default n
                    config OS_VCOM_SERNO
                        string "serial number of virtual com"
                        default "32021919830108"
                    config OS_VCOM_SER_LEN
                        int "serial number length of virtual com"
                        default 14
                    config OS_VCOM_TX_TIMEOUT
                        int "tx timeout(ticks) of virtual com"
                        default 1000
                endif
                if OS_USB_DEVICE_WINUSB
                    config OS_WINUSB_GUID
                    string "Guid for winusb"
                    default "{6860DC3C-C05F-4807-8807-1CA861CC1D66}"
                endif
                if OS_USB_DEVICE_MSTORAGE
                    config OS_USB_MSTORAGE_DISK_NAME
                    string "msc class disk name"
                    default "flash0"
                endif

                if OS_USB_DEVICE_RNDIS
                    config RNDIS_DELAY_LINK_UP
                        bool "Delay linkup media connection"
                        select OS_USING_TIMER_SOFT
                        default n
                endif

                if OS_USB_DEVICE_HID
                    config OS_USB_DEVICE_HID_KEYBOARD
                        bool "Use to HID device as Keyboard"
                        default n
                    if OS_USB_DEVICE_HID_KEYBOARD
                        config OS_USB_DEVICE_HID_KEYBOARD_NUMBER
                        int "Number of Keyboard(max 3)"
                        default 1
                        range 1 3
                    endif
                    config OS_USB_DEVICE_HID_MOUSE
                        bool "Use to HID device as Mouse"
                        default n
                    config OS_USB_DEVICE_HID_GENERAL
                        bool "Use to HID device as General HID device"
                        default y
                        if OS_USB_DEVICE_HID_GENERAL
                            config OS_USB_DEVICE_HID_GENERAL_OUT_REPORT_LENGTH
                                int "General HID device out report length"
                                default 63
                                range 0 63

                            config OS_USB_DEVICE_HID_GENERAL_IN_REPORT_LENGTH
                                int "General HID device in report length"
                                default 63
                                range 0 63
                        endif
                    config OS_USB_DEVICE_HID_MEDIA
                        bool "Use to HID device as media keyboard"
                        default y
                endif
                if OS_USB_DEVICE_AUDIO
                    config OS_USB_DEVICE_AUDIO_MIC
                        bool "Use usb mic device as audio device"
                        default n
                        if OS_USB_DEVICE_AUDIO_MIC
                            config OS_USBD_MIC_DEVICE_NAME
                            string "audio mic device name"
                            default "mic0"
                        endif
                    config OS_USB_DEVICE_AUDIO_SPEAKER
                        bool "Use usb speaker device as audio device"
                        default n
                        if OS_USB_DEVICE_AUDIO_SPEAKER
                            config OS_USBD_SPEAKER_DEVICE_NAME
                            string "audio speaker device name"
                            default "sound0"
                        endif
                endif
        endif
endmenu