config BSP_USING_WIFI_AP6181
    bool "Enable Wi-Fi AP6181"
    select OS_USING_SDIO
    select OS_USING_WIFI
    select OS_WLAN_PROT_LWIP_PBUF_FORCE
    select OS_USING_LWIP
    select OS_USING_LIBC
    select OS_USING_POSIX
    select OS_USING_VFS
    select OS_USING_SAL
    select OS_USING_RTTHREAD_ADAPTER
    default n

    if BSP_USING_WIFI_AP6181
        config BSP_AP6181_REG_ON_PIN
            int "AP6181 wifi reg on pin"
            default 49
        config BSP_AP6181_IRQ_PIN
            int "AP6181 interrupt pin"
            default 37
    endif