menu "Kernel"

    choice
        prompt "The max size of kernel object name"
        default OS_NAME_MAX_15

        config OS_NAME_MAX_7
            bool "7"

        config OS_NAME_MAX_15
            bool "15"

        config OS_NAME_MAX_31
            bool "31"
    endchoice
    config OS_NAME_MAX
        int
        default 7  if OS_NAME_MAX_7
        default 15 if OS_NAME_MAX_15
        default 31 if OS_NAME_MAX_31

    config OS_ALIGN_SIZE
        int "Alignment size for CPU architecture data access"
        default 4
        help
            Alignment size for CPU architecture data access

    choice
        prompt "The max level value of priority of task"
        default OS_TASK_PRIORITY_32

        config OS_TASK_PRIORITY_8
            bool "8"
        config OS_TASK_PRIORITY_32
            bool "32"
        config OS_TASK_PRIORITY_256
            bool "256"
    endchoice
    config OS_TASK_PRIORITY_MAX
        int
        default 8   if OS_TASK_PRIORITY_8
        default 32  if OS_TASK_PRIORITY_32
        default 256 if OS_TASK_PRIORITY_256

    config OS_TICK_PER_SECOND
        int "Tick frequency(Hz)"
        range 10 1000
        default 100
        help
            System's tick frequency(Hz).

    config OS_USING_OVERFLOW_CHECK
        bool "Using stack overflow checking"
        default y
        help
            Enable task stack overflow checking. The stack overflow is checking when
            each task switch.

	config OS_MAIN_TASK_STACK_SIZE
        int "The stack size of main task"
        default 2048
		
    config OS_USING_HOOK
        bool "Enable system hook"
        default y
        select OS_USING_IDLE_HOOK
        help
            Enable the hook function when system running, such as idle task hook,
            task context switch etc.

    config OS_USING_IDLE_HOOK
        bool "Enable idle task hook"
        default y if OS_USING_HOOK

        if OS_USING_IDLE_HOOK
            config OS_IDLE_HOOK_LIST_SIZE
                int "The max size of idle hook list"
                default 4
                range 1 16
                help
                    The system has a hook list. This is the hook list size.
        endif

    config OS_IDLE_TASK_STACK_SIZE
        int "The stack size of idle task"
        default 512

    config OS_USING_TIMER_SOFT
        bool "Enable software timer with a timer task"
        default y
        help
            The timeout function context of soft-timer is under a high priority timer
            task.

        if OS_USING_TIMER_SOFT
            config OS_TIMER_TASK_PRIO
                int "The priority level value of timer task"
                default 0

            config OS_TIMER_TASK_STACK_SIZE
                int "The stack size of timer task"
                default 512
        endif

    config OS_USING_WORKQUEUE
        bool "Enable workqueue"
        depends on OS_USING_HEAP
        default y
            
        if OS_USING_WORKQUEUE
            config OS_USING_SYSTEM_WORKQUEUE
                bool "Enable system workqueue"
                default y
                
            if OS_USING_SYSTEM_WORKQUEUE
                config OS_SYSTEM_WORKQUEUE_STACK_SIZE
                    int "System workqueue task stack size"
                    default 2048
                    
                config OS_SYSTEM_WORKQUEUE_PRIORITY
                    int "System workqueue task priority level"
                    default 3  if OS_TASK_PRIORITY_8
                    default 8  if OS_TASK_PRIORITY_32
                    default 20 if OS_TASK_PRIORITY_256
            endif
        endif
        
    if OS_USING_LIBC && OS_USING_VFS    
        config OS_USING_MODULE
            bool "Enable kernel module"
            default n
            help
                Using kernel module and shared library.
    endif
    
    menu "Task communication"
        config OS_USING_SEMAPHORE
            bool "Enable semaphore"
            default y

        config OS_USING_MUTEX
            bool "Enable mutex"
            default y

        config OS_USING_EVENT
            bool "Enable event flag"
            default y

        config OS_USING_MAILBOX
            bool "Enable mailbox"
            default y

        config OS_USING_MESSAGEQUEUE
            bool "Enable message queue"
            default y

        config OS_USING_COMPLETION
            bool "Enable completion"
            default y
        
        config OS_USING_DATAQUEUE
            bool "Enable dataqueue"
            depends on OS_USING_HEAP
            default y
        config OS_USING_WAITQUEUE
            bool "Enable waitqueue"
            default y
    endmenu

    menu "Memory management"
        config OS_USING_MEM_POOL
            bool "Using memory pool"
            default y
            help
                Using static memory fixed partition

        config OS_USING_MEM_HEAP
            bool "Using memory heap object"
            default n
            help
                Using memory heap object to manage dynamic memory heap.

        choice
            prompt "Dynamic memory management"
            default OS_USING_MEM_SMALL

            config OS_USING_NO_HEAP
                bool "Disable heap"
            config OS_USING_MEM_SMALL
                bool "Small memory algorithm for small memory"
            config OS_USING_MEM_SLAB
                bool "SLAB algorithm for large memory"
            if OS_USING_MEM_HEAP
                config OS_USING_MEM_HEAP_AS_HEAP
                    bool "Use all of memheap objects as heap"
            endif
        endchoice
        config OS_USING_HEAP
            bool
            default n if OS_USING_NO_HEAP
            default y if OS_USING_MEM_SMALL
            default y if OS_USING_MEM_SLAB
            default y if OS_USING_MEM_HEAP_AS_HEAP
        
        if OS_USING_MEM_SMALL || OS_USING_MEM_SLAB || OS_USING_MEM_HEAP_AS_HEAP
            config OS_MEM_STATS
                bool "Enable memory stats"
                default y
        endif
        
        if OS_USING_MEM_SMALL
            config OS_USING_MEMTRACE
                bool "Enable memory trace"
                default n
                help
                    When enable OS_USING_MEMTRACE with shell, developer can call cmd:
                    1. memtrace
                       to dump memory block information.
                    2. memcheck
                       to check memory block to avoid memory overwritten.

                    And developer also can call memcheck() in each of scheduling
                    to check memory block to find which thread has wrongly modified
                    memory.
        endif
    endmenu

    menu "Kernel console"
        config OS_USING_CONSOLE
            bool "Using console for os_kprintf"
            default y

        if OS_USING_CONSOLE
            config OS_CONSOLE_DEVICE_NAME
                string "The device name for console"
                default "uart1"
        endif  
    endmenu

    menu "Enable assert"
        config OS_USING_ASSERT
            bool "Enable global assert"
            default y
    endmenu
    
    if OS_DEBUG
        menu "Kernel debug"
            config OS_USING_KERNEL_DEBUG
                bool "Enable kernel debug"
                default y
            
            if OS_USING_KERNEL_DEBUG
                config OS_USING_CONTEXT_CHECK
                bool "Enable check context"
                default n       
            endif

            choice
                prompt "The global log level of kernel"
                default KLOG_GLOBAL_LEVEL_WARNING

                config KLOG_GLOBAL_LEVEL_ERROR
                    bool "Error"
                config KLOG_GLOBAL_LEVEL_WARNING
                    bool "Warning"
                config KLOG_GLOBAL_LEVEL_INFO
                    bool "Infomation"
                config KLOG_GLOBAL_LEVEL_DEBUG
                    bool "Debug"
            endchoice
            config KLOG_GLOBAL_LEVEL
                int
                default 0 if KLOG_GLOBAL_LEVEL_ERROR
                default 1 if KLOG_GLOBAL_LEVEL_WARNING
                default 2 if KLOG_GLOBAL_LEVEL_INFO
                default 3 if KLOG_GLOBAL_LEVEL_DEBUG
                
            config KLOG_USING_COLOR
                bool "Enable color log"
                default y
                help
                    The log will has different color by level
        endmenu
    endif
endmenu