import os
Import('osconfig')
from build_tools import *

pwd  = PresentDir()
src  = []
list = os.listdir(pwd)

CPPPATH    = []
CPPDEFINES = []
LIBS       = []

#add common header files
CPPPATH.append(pwd + '/include')

#gcc with newlib
if osconfig.COMPILER == 'gcc' and IsDefined('OS_USING_LIBC'):
    CPPDEFINES += ['OS_USING_NEWLIB']
    CPPPATH.append(pwd + '/include/newlib')
    src += Glob('source/newlib/*.c')
    src += Glob('source/common/*.c')
    
    # link with libc and libm:
    # libm is a frequently used lib. Newlib is compiled with -ffunction-sections in
    # recent GCC tool chains. The linker would just link in the functions that have
    # been referenced. So setting this won't result in bigger text size.
    LIBS += ['c', 'm']

#gcc with armlibc    
if (osconfig.COMPILER == 'armcc' or osconfig.COMPILER == 'armclang') and IsDefined('OS_USING_LIBC'):
    CPPDEFINES += ['OS_USING_ARM_LIBC']
    CPPPATH.append(pwd + '/include/armlibc')
    src += Glob('source/armlibc/*.c')
    src += Glob('source/common/*.c')

#gcc with dlib
if osconfig.COMPILER == 'iar' and IsDefined('OS_USING_LIBC'):
    CPPDEFINES += ['OS_USING_DLIBC']
    CPPPATH.append(pwd + '/include/dlib')
    src += Glob('source/dlib/*.c')
    src += Glob('source/common/*.c')

    if IsDefined('OS_USING_DFS'):
        from distutils.version import LooseVersion
        from iar import IARVersion

        CPPDEFINES += ['_DLIB_FILE_DESCRIPTOR']

        if LooseVersion(IARVersion()) < LooseVersion("8.20.1"):
            CPPDEFINES += ['_DLIB_THREAD_SUPPORT']

group = AddCodeGroup('libc', src, depend = [''], CPPPATH = CPPPATH, CPPDEFINES = CPPDEFINES, LIBS = LIBS)

Return('group')