# Common application source files.
set( DEMO_APP_SOURCES
     app/iot_demo.c
     app/iot_demo_arguments.c )

# When testing the demos, add the test sources and redefine the demo main function.
if( ${IOT_BUILD_TESTS} )
    list( APPEND DEMO_APP_SOURCES ${PROJECT_SOURCE_DIR}/tests/iot_tests.c )
    set_property( SOURCE app/iot_demo.c PROPERTY COMPILE_DEFINITIONS main=DemoMain )
    set( CONFIG_HEADER ${PROJECT_SOURCE_DIR}/tests/iot_config.h )
else()
    set( CONFIG_HEADER iot_config.h )
endif()

# Common demo header files.
set( DEMO_COMMON_HEADERS
     include/iot_demo_arguments.h
     include/iot_demo_logging.h )

# List all the demo functions, source files, and library dependencies here.
#
# The list order matters: Each demo must be at the same index in each list.
# For example, if the MQTT demo function is at DEMO_MAIN_FUNCTIONS[0], then
# the MQTT demo source must be at DEMO_SOURCES[0] and the MQTT library must
# be at DEMO_LIBRARY_DEPENDENCY[0].
#
# If a demo has multiple dependencies, place a semicolon-separated list in
# DEMO_LIBRARY_DEPENDENCY. The semicolon itself must be escaped as \\\;
set( DEMO_MAIN_FUNCTIONS
     RunMqttDemo
     RunShadowDemo
     RunDefenderDemo
     RunJobsDemo
     RunProvisioningWithKeysAndCertDemo
     RunProvisioningWithCsrDemo )
set( DEMO_SOURCES
     src/iot_demo_mqtt.c
     src/aws_iot_demo_shadow.c
     src/aws_iot_demo_defender.c
     src/aws_iot_demo_jobs.c
     src/Provisioning/aws_iot_demo_provisioning_with_keys_and_cert.c
     src/Provisioning/aws_iot_demo_provisioning_with_csr.c )

set( DEMO_LIBRARY_DEPENDENCY
     iotmqtt
     "awsiotshadow\\\;awsiotcommon"
     awsiotdefender 
     "awsiotjobs\\\;awsiotcommon"  
     "awsiotprovisioning\\\;awsiotcommon" 
     "awsiotprovisioning\\\;awsiotcommon" )

# Get the list length to iterate over it. Since CMake indexes from 0, subtract
# 1 for the iteration range.
list( LENGTH DEMO_MAIN_FUNCTIONS DEMO_COUNT )
math( EXPR DEMO_COUNT "${DEMO_COUNT}-1" )

# Go through the list of demos and create an executable for each one.
foreach( i RANGE ${DEMO_COUNT} )
    # Read the demo function, source, and dependency from each list.
    list( GET DEMO_MAIN_FUNCTIONS ${i} CURRENT_DEMO_FUNCTION )
    list( GET DEMO_SOURCES ${i} CURRENT_DEMO_SOURCE )
    list( GET DEMO_LIBRARY_DEPENDENCY ${i} CURRENT_DEMO_LIBRARY )

    # Get the name of the demo executable. This is the name of the demo source
    # without the .c file extension.
    get_filename_component( DEMO_EXE_NAME ${CURRENT_DEMO_SOURCE} NAME_WE )

    # Add the demo executable.
    add_executable( ${DEMO_EXE_NAME}
                    ${CURRENT_DEMO_SOURCE}
                    ${DEMO_APP_SOURCES}
                    ${DEMO_COMMON_HEADERS}
                    ${CONFIG_HEADER} )

    # Set the demo function to run.
    target_compile_definitions( ${DEMO_EXE_NAME}
                                PRIVATE RunDemo=${CURRENT_DEMO_FUNCTION} )

    # Set additional defines when testing the demos.
    if( ${IOT_BUILD_TESTS} )
        target_compile_definitions( ${DEMO_EXE_NAME} PRIVATE
                                    IOT_TEST_DEMO=1 )
    endif()

    # Add the include path for the demo application.
    target_include_directories( ${DEMO_EXE_NAME} PRIVATE include )

    # Link iotbase. All demos require this.
    target_link_libraries( ${DEMO_EXE_NAME} PRIVATE iotbase )

    # Link the unique dependency of each demo.
    target_link_libraries( ${DEMO_EXE_NAME} PRIVATE ${CURRENT_DEMO_LIBRARY} )

    # When building tests, link the Unity test framework.
    if( ${IOT_BUILD_TESTS} )
        target_link_libraries( ${DEMO_EXE_NAME} PRIVATE unity )
    endif()

    # Organize the demo into folders.
    set_property( TARGET ${DEMO_EXE_NAME} PROPERTY FOLDER demos )
    source_group( app FILES ${DEMO_APP_SOURCES} )
    source_group( include FILES ${DEMO_COMMON_HEADERS} )
    source_group( src FILES ${CURRENT_DEMO_SOURCE} )
    source_group( "" FILES ${CONFIG_HEADER} )
endforeach()