# Kconfig file for package ali-iotkit
menu "Ali-iotkit"
    config PKG_USING_ALI_IOTKIT
    bool "Ali-iotkit: Aliyun cloud sdk 'iotkit-embedded'"
    select NET_USING_BSD    
    default n

if PKG_USING_ALI_IOTKIT

    choice
        prompt "Version"
        default PKG_USING_ALI_IOTKIT_V30100
        help
            Select the ali-iotkit version

        config PKG_USING_ALI_IOTKIT_V30100
            bool "v3.1.0"
    endchoice
    
    config PKG_USING_ALI_IOTKIT_PRODUCT_KEY
        string "Config Product Key"
        default "a1mFunc9SVl"

    config PKG_USING_ALI_IOTKIT_PRODUCT_SECRET
        string "Config Product Secret"
        default "*******"

    config PKG_USING_ALI_IOTKIT_DEVICE_NAME
        string "Config Device Name"
        default "dev_0"        

    config PKG_USING_ALI_IOTKIT_DEVICE_SECRET
        string "Config Device Secret"
        default "4mevyxGE6CGCGX8kL6dGWIyIj7Gq31tj"

    config PKG_ALI_IOTKIT_SELECT_ITEM
        bool
        select PLATFORM_HAS_OS
        select PLATFORM_HAS_STDINT
        default y
        
    if PKG_USING_ALI_IOTKIT_V30100
        source "$OS_ROOT/thirdparty/Aliiotkit-v3.1.0/tools/menu/Config.infra"
        source "$OS_ROOT/thirdparty/Aliiotkit-v3.1.0/tools/menu/Config.dev_sign"
        source "$OS_ROOT/thirdparty/Aliiotkit-v3.1.0/tools/menu/Config.mqtt"
        source "$OS_ROOT/thirdparty/Aliiotkit-v3.1.0/tools/menu/Config.dynamic_register"
        source "$OS_ROOT/thirdparty/Aliiotkit-v3.1.0/tools/menu/Config.dev_model"
        source "$OS_ROOT/thirdparty/Aliiotkit-v3.1.0/tools/menu/Config.wrappers"
        source "$OS_ROOT/thirdparty/Aliiotkit-v3.1.0/tools/menu/Config.ota"
        source "$OS_ROOT/thirdparty/Aliiotkit-v3.1.0/tools/menu/Config.coap"
        source "$OS_ROOT/thirdparty/Aliiotkit-v3.1.0/tools/menu/Config.dev_reset"
        source "$OS_ROOT/thirdparty/Aliiotkit-v3.1.0/tools/menu/Config.http"
        source "$OS_ROOT/thirdparty/Aliiotkit-v3.1.0/tools/menu/Config.http2"
        source "$OS_ROOT/thirdparty/Aliiotkit-v3.1.0/tools/menu/Config.wifi_provision"
        source "$OS_ROOT/thirdparty/Aliiotkit-v3.1.0/tools/menu/Config.dev_bind"
    endif
    
    config PKG_USING_ALI_IOTKIT_SAMPLES
        bool "Samples"
        default n 

    if PKG_USING_ALI_IOTKIT_SAMPLES
        config PKG_USING_ALI_IOTKIT_MQTT_SAMPLE
            bool "Enable MQTT sample"
            depends on MQTT_COMM_ENABLED
            default y
        config PKG_USING_ALI_IOTKIT_COAP_SAMPLE
            bool "Enable COAP sample"
            depends on COAP_COMM_ENABLED
            default n
        config PKG_USING_ALI_IOTKIT_OTA_SAMPLE
            bool "Enable OTA sample"
            depends on OTA_ENABLED
            default n
    endif


endif
endmenu