menu "MicroPython"
menuconfig PKG_USING_MICROPYTHON
    bool "Enable MicroPython"
	select OS_USING_CONSOLE
	select OS_USING_DEVICE
	select OS_USING_LIBC
	select OS_USING_VFS
    default n
	
	if PKG_USING_MICROPYTHON

#==========================================================================

		menu "Hardware information"
			config MICROPY_HW_MCU_NAME
				string "Set micropython mcu name"
				default "stm32l475"
				
			config MICROPYTHON_RAM_SIZE
				int "The maximum memory size of micropython (KB)"
	            default 32
			
			config MICROPYTHON_RAM_START
				hex "The start memory adress of micropython"
	            default 0x10000000
			
		endmenu

#==========================================================================		
			
		menuconfig PKG_MICROPYTHON_MACHINE_BUS
			bool "machine: Enable micropython machine module"
			default n
			
		if PKG_MICROPYTHON_MACHINE_BUS
			config MICROPY_PY_ADC
				bool "adc: Enable micropython machine module"
				select OS_USING_ADC
				default n
			if MICROPY_PY_ADC
				config MICROPYTHON_MACHINE_ADC_PRENAME
					string "similar adc devices prename"
					default "adc"
			endif	
			
			config MICROPY_PY_CAN
				bool "can: Enable micropython machine module"
				select OS_USING_CAN
				default n
			if MICROPY_PY_CAN
				config MICROPYTHON_MACHINE_CAN_PRENAME
					string "Set similar can devices prename"
					default "can"
			endif	
			
			config MICROPY_PY_DAC
				bool "dac: Enable micropython machine module"
				select OS_USING_DAC
				default n
			if MICROPY_PY_DAC
				config MICROPYTHON_MACHINE_DAC_PRENAME
					string "Set similar dac devices prename"
					default "dac"
			endif
			
			config MICROPY_PY_I2C
				bool "i2c: Enable micropython machine module"
				select OS_USING_I2C
				default n
			if MICROPY_PY_I2C
				config MICROPYTHON_MACHINE_I2C_PRENAME
					string "Set similar i2c devices prename"
					default "i2c"
			endif
			
			config MICROPY_PY_SPI
				bool "spi: Enable micropython machine module"
				select MICROPY_PY_PIN
				select OS_USING_SPI
				default n
			if MICROPY_PY_SPI
				config MICROPYTHON_MACHINE_SPI_PRENAME
					string "Set similar spi devices prename"
					default "spi"
			endif
			
			config MICROPY_PY_UART
				bool "uart: Enable micropython machine module"
				select OS_USING_SERIAL
				default n
			if MICROPY_PY_UART
				config MICROPYTHON_MACHINE_UART_PRENAME
					string "Set similar uart devices prename"
					default "uart"
			endif
			
			config MICROPY_PY_PWM
				bool "pwm: Enable micropython machine module"
				select OS_USING_PWM
				default n
			if MICROPY_PY_PWM
				config MICROPYTHON_MACHINE_PWM_PRENAME
					string "Set similar pwm devices prename"
					default "pwm"
			endif
			
			config MICROPY_PY_WDT
				bool "wdt: Enable micropython machine module"
				select OS_USING_WDG
				default n
			if MICROPY_PY_WDT
				config MICROPYTHON_MACHINE_WDT_NAME
					string "Set wdt device name"
					default "iwdg"
			endif

			config MICROPY_PY_PIN
				bool "pin: Enable micropython machine module"
				select OS_USING_PIN
				default n

			config MICROPY_PY_RTC
				bool "rtc: Enable micropython machine module"
				select OS_USING_RTC
				default n		
			
			config MICROPY_PY_TIMER
				bool "timer: Enable micropython machine module"
				default n
			
			config MICROPY_PY_PM
				bool "pm: Enable micropython machine module"
				select OS_USING_LPMGR
				default n
		endif

#==========================================================================

		menuconfig PKG_MICROPYTHON_DEVICE
			bool "device: Enable micropython device module"
			default n
			
		if PKG_MICROPYTHON_DEVICE
			config MICROPY_DEVICE_AUDIO
				bool "audio: Enable device module"
				default n
			if MICROPY_DEVICE_AUDIO
				config MICROPYTHON_DEVICE_AUDIO_NAME
					string "Set audio device name"
					default "audio0"
			endif
			
			config MICROPY_DEVICE_BEEP
				bool "beep: Enable device module"
				default n
			
			config MICROPY_DEVICE_KEY
				bool "key: Enable device module"
				default n
			
			config MICROPY_DEVICE_LCD
				bool "lcd: Enable device module"
				default n
			
			config MICROPY_DEVICE_LED
				bool "led: Enable device module"
				default n
			
			config MICROPY_DEVICE_HUMITURE
				bool "humiture: Enable sensor module"
				default n
			if MICROPY_DEVICE_HUMITURE
				config MICROPYTHON_DEVICE_HUMIDITY_NAME
					string "Set humidity sensor name"
					default "humi_aht10"
				
				config MICROPYTHON_DEVICE_TEMPERATURE_NAME
					string "Set temperature sensor name"
					default "temp_aht10"
			endif
			
			config MICROPY_DEVICE_SIX_AXIS
				bool "six_axis: Enable sensor module"
				default n
			if MICROPY_DEVICE_SIX_AXIS
				config MICROPYTHON_DEVICE_GGYROSCOPE_NAME
					string "Set gyroscope sensor name"
					default "gyro_icm20602"
					
				config MICROPYTHON_DEVICE_ACCELEROMETER_NAME
					string "Set accelerometer sensor name"
					default "acce_icm20602"
			endif
			
			config MICROPY_DEVICE_LIGHTSENSOR
				bool "lightsensor: Enable sensor module"
				default n
			if MICROPY_DEVICE_LIGHTSENSOR
				config MICROPYTHON_DEVICE_LIGHTSENSOR_NAME
					string "Set light sensor name"
					default "li_ap3216c"
			endif
			
		endif

#==========================================================================

		 menu "Micropython std-libs and micro-libs"
	        config MICROPY_USING_MATH
	            bool "math: mathematical functions"
	            default n
	        if MICROPY_USING_MATH
	        	config MICROPY_USING_MATH_SPECIAL_FUNCTIONS
					bool "provide special math functions: math.{erf,erfc,gamma,lgamma}"
					default n
					
				config MICROPY_USING_MATH_FACTORIAL
					bool "provide math.factorial function"
					default n
					
				config MICROPY_USING_MATH_ISCLOSE
					bool "provide math.isclose function"
					default n
			endif

			
	        config MICROPY_USING_UBINASCII
	            bool "ubinascii: binary/ASCII conversions"
	            default n
	        if MICROPY_USING_UBINASCII
	           	config MICROPY_USING_UBINASCII_CRC32
	           	bool "Compute CRC-32"
	           	default n
	        endif  


	        config MICROPY_USING_COLLECTIONS
	            bool "ucollectsions: collection and container types"
	            default n
	        if MICROPY_USING_COLLECTIONS
	           	config MICROPY_USING_COLLECTIONS_DEQUE
	           	bool "provide ucollections.deque type"
	           	default n

	           	config MICROPY_USING_COLLECTIONS_ORDEREDDICT
	           	bool "provide ucollections.OrderedDict type"
	           	default n

	           	config MICROPY_USING_COLLECTIONS_NAMEDTUPLE__ASDICT
	           	bool "provide the _asdict function for namedtuple"
	           	select MICROPY_USING_COLLECTIONS_ORDEREDDICT
	           	default n
	        endif 

			#---------------- 
			if 0
			config MICROPY_USING_ARRAY
	            bool "uarray: arrays of numeric data"
	            default n


	        config MICROPY_USING_UHASHLIB
	            bool "uhashlib: hashing algorithms"
	            default n
	        if MICROPY_USING_UHASHLIB
	          	config MICROPY_USING_UHASHLIB_MD5
	          	bool "provide MD5 algorithms"
	         	default n
            
	          	config MICROPY_USING_UHASHLIB_SHA1
              	bool "provide SHA1 algorithms"
              	default n
            
              	config MICROPY_USING_UHASHLIB_SHA256
              	bool "provide SHA256 algorithms"
              	default n
            endif
            endif 
			#---------------- 

	        config MICROPY_USING_UHEAPQ
	            bool "uheapq: heap queue algorithm"
	            default n


	        config MICROPY_USING_UJSON
	            bool "ujson: JSON encoding and decoding"
	            default n


	        config MICROPY_USING_URE
	            bool "ure: simple regular expressions"
	            default n
            if MICROPY_USING_URE
	           config MICROPY_USING_URE_DEBUG
	           bool "provide ure.DEBUG function"
	           default n
            
	           config MICROPY_USING_URE_MATCH_GROUPS
               bool "provide groups function for ure.match/search"
               default n
            
               config MICROPY_USING_URE_MATCH_SPAN_START_END
               bool "provide span/start/end function for ure.match/search"
               default n

               config MICROPY_USING_URE_SUB
               bool "provide ure.sub function"
               default n
            endif 


	        config MICROPY_USING_UZLIB
	            bool "uzlib: zlib decompression"
	            default n

    	endmenu
#==========================================================================


        menu "Micropython components"
			if 0
			config MICROPY_USING_AMS
				bool "Enable micropython application management system" 
				default n
			if MICROPY_USING_AMS
				config MICROPY_FS_DEVICE_NAME
					string "Set file system device(SD,W25Q64, etc)"
					default "sd0"
			endif
			
			config MICROPY_PY_ONENET
				bool "Enable micropython onenet module"
				default n
			endif
		endmenu

#==========================================================================
	endif
	
	
endmenu