menu "mbedTLS"

config MBEDTLS_SSL_MAX_CONTENT_LEN
    int "TLS maximum message content length"
    default 16384
    range 512 16384
    help
        Maximum TLS message length (in bytes) supported by mbedTLS.
        
        16384 is the default and this value is required to comply
        fully with TLS standards.
        
        However you can set a lower value in order to save RAM. This
        is safe if the other end of the connection supports Maximum
        Fragment Length Negotiation Extension (max_fragment_length,
        see RFC6066) or you know for certain that it will never send a
        message longer than a certain number of bytes.
        
        If the value is set too low, symptoms are a failed TLS
        handshake or a return value of MBEDTLS_ERR_SSL_INVALID_RECORD
        (-0x7200).

config MBEDTLS_DEBUG
   bool "Enable mbedTLS debugging"
   default n
   help
       Enable mbedTLS debugging functions at compile time.

       If this option is enabled, you can include
	   "mbedtls/esp_debug.h" and call mbedtls_esp_enable_debug_log()
	   at runtime in order to enable mbedTLS debug output via the ESP
	   log mechanism.

config MBEDTLS_HARDWARE_AES
   bool "Enable hardware AES acceleration"
   default y
   help
       Enable hardware accelerated AES encryption & decryption.

config MBEDTLS_HARDWARE_MPI
   bool "Enable hardware MPI (bignum) acceleration"
   default y
   help
       Enable hardware accelerated multiple precision integer operations.

       Hardware accelerated multiplication, modulo multiplication,
       and modular exponentiation for up to 4096 bit results.

       These operations are used by RSA.

config MBEDTLS_MPI_USE_INTERRUPT
    bool "Use interrupt for MPI operations"
    depends on MBEDTLS_HARDWARE_MPI
    default y
    help
        Use an interrupt to coordinate MPI operations.

        This allows other code to run on the CPU while an MPI operation is pending.
        Otherwise the CPU busy-waits.

config MBEDTLS_HARDWARE_SHA
   bool "Enable hardware SHA acceleration"
   default y
   help
       Enable hardware accelerated SHA1, SHA256, SHA384 & SHA512 in mbedTLS.

       Due to a hardware limitation, hardware acceleration is only
       guaranteed if SHA digests are calculated one at a time. If more
       than one SHA digest is calculated at the same time, only will
       be calculated fully in hardware and the rest will be calculated
       (at least partially calculated) in software.

config MBEDTLS_HAVE_TIME
   bool "Enable mbedtls time"
   depends on !ESP32_TIME_SYSCALL_USE_NONE
   default y
   help
       System has time.h and time().
       The time does not need to be correct, only time differences are used,

config MBEDTLS_HAVE_TIME_DATE
   bool "Enable mbedtls time data"
   depends on MBEDTLS_HAVE_TIME
   default n
   help
       System has time.h and time(), gmtime() and the clock is correct.
       The time needs to be correct (not necesarily very accurate, but at least
       the date should be correct). This is used to verify the validity period of
       X.509 certificates.

       It is suggested that you should get the real time by "SNTP".

endmenu