# This is Doxygen configuration file
#
# Doxygen provides over 260 configuration statements
# To make this file easier to follow,
# it contains only statements that are non-default
#
# NOTE:
# It is recommended not to change defaults unless specifically required
# Test any changes how they affect generated documentation
# Make sure that correct warnings are generated to flag issues with documented code
#
# For the complete list of configuration statements see:
# http://www.stack.nl/~dimitri/doxygen/manual/config.html


PROJECT_NAME = "ESP32 Programming Guide"

## The 'INPUT' statement below is used as input by script 'gen-df-input.py'
## to automatically generate API reference list files heder_file.inc
## These files are placed in '_inc' directory
## and used to include in API reference documentation

INPUT = \
    ##
    ## Wi-Fi - API Reference
    ##
    ../components/esp32/include/esp_wifi.h \
    ../components/esp32/include/esp_smartconfig.h \
    ## Bluetooth - API Reference
    ## Controller && VHCI
    ../components/bt/include/bt.h \
    ## Bluetooth COMMON
    ## Issue with __attribute__
    ../components/bt/bluedroid/api/include/esp_bt_defs.h \
    ../components/bt/bluedroid/api/include/esp_bt_main.h \
    ../components/bt/bluedroid/api/include/esp_bt_device.h \
    ## Bluetooth LE
    ../components/bt/bluedroid/api/include/esp_gap_ble_api.h \
    ## Issue with __attribute__
    ../components/bt/bluedroid/api/include/esp_gatt_defs.h \
    ../components/bt/bluedroid/api/include/esp_gatts_api.h \
    ../components/bt/bluedroid/api/include/esp_gattc_api.h \
    ../components/bt/bluedroid/api/include/esp_blufi_api.h \
    ## Bluetooth Classic
    ../components/bt/bluedroid/api/include/esp_gap_bt_api.h \
    ## Issue with __attribute__
    ../components/bt/bluedroid/api/include/esp_a2dp_api.h \
    ../components/bt/bluedroid/api/include/esp_avrc_api.h \
    ##
    ## Ethernet - API Reference
    ##
    ../components/ethernet/include/esp_eth.h \
    ../components/ethernet/include/eth_phy/phy.h \
    ../components/ethernet/include/eth_phy/phy_tlk110.h \
    ../components/ethernet/include/eth_phy/phy_lan8720.h \
    ##
    ## Peripherals - API Reference
    ##
    ../components/driver/include/driver/adc.h \
    ../components/driver/include/driver/dac.h \
    ../components/driver/include/driver/gpio.h \
    ../components/driver/include/driver/rtc_io.h \
    ../components/driver/include/driver/i2c.h \
    ../components/driver/include/driver/i2s.h \
    ../components/driver/include/driver/ledc.h \
    ../components/driver/include/driver/mcpwm.h \
    ../components/driver/include/driver/pcnt.h \
    ../components/driver/include/driver/rmt.h \
    ../components/driver/include/driver/sigmadelta.h \
    ../components/driver/include/driver/spi_common.h \
    ../components/driver/include/driver/spi_master.h \
    ../components/driver/include/driver/spi_slave.h \
    ../components/driver/include/driver/timer.h \
    ../components/driver/include/driver/uart.h \
    ##
    ## Protocols - API Reference
    ##
    ../components/mdns/include/mdns.h \
    ##
    ## Storage - API Reference
    ##
    ## SPI Flash and Partition APIs
    ../components/spi_flash/include/esp_spi_flash.h \
    ../components/spi_flash/include/esp_partition.h \
    ../components/bootloader_support/include/esp_flash_encrypt.h \
    ## SD/MMC Card Host
    ## NOTE: for three lines below header_file.inc is not used
    ../components/sdmmc/include/sdmmc_cmd.h \
    ../components/driver/include/driver/sdmmc_host.h \
    ../components/driver/include/driver/sdmmc_types.h \
    ## Non-Volatile Storage
    ../components/nvs_flash/include/nvs.h \
    ../components/nvs_flash/include/nvs_flash.h \
    ## Virtual Filesystem
    ../components/vfs/include/esp_vfs.h \
    ../components/vfs/include/esp_vfs_dev.h \
    ## FAT Filesystem
    ## NOTE: for two lines below header_file.inc is not used
    ../components/fatfs/src/esp_vfs_fat.h \
    ../components/fatfs/src/diskio.h \
    ## Wear Levelling
    ../components/wear_levelling/include/wear_levelling.h \
    ##
    ## System - API Reference
    ##
    ## Memory Allocation    #
    ../components/esp32/include/esp_heap_alloc_caps.h \
    ../components/freertos/include/freertos/heap_regions.h \
    ## Interrupt Allocation
    ../components/esp32/include/esp_intr_alloc.h \
    ## Watchdogs
    ## NOTE: for two lines below header_file.inc is not used
    ../components/esp32/include/esp_int_wdt.h \
    ../components/esp32/include/esp_task_wdt.h \
    ## Over The Air Updates (OTA)
    ../components/app_update/include/esp_ota_ops.h \
    ## Deep Sleep
    ## NOTE: for line below header_file.inc is not used
    ../components/esp32/include/esp_deep_sleep.h \
    ## Logging
    ../components/log/include/esp_log.h \
    ## Base MAC address
    ## NOTE: for line below header_file.inc is not used
    ../components/esp32/include/esp_system.h \
    ##
    ## ULP Coprocessor - API Guides
    ##
    ## NOTE: for line below header_file.inc is not used
    ../components/ulp/include/esp32/ulp.h \
    ##
    ## Application Level Tracing - API Reference
    ##
    ../components/app_trace/include/esp_app_trace.h


## Get warnings for functions that have no documentation for their parameters or return value
##
WARN_NO_PARAMDOC = YES

## Enable preprocessing and remove __attribute__(...) expressions from the INPUT files
##
ENABLE_PREPROCESSING   = YES
MACRO_EXPANSION        = YES
EXPAND_ONLY_PREDEF     = YES
PREDEFINED             = __attribute__(x)=

## Do not complain about not having dot
##
HAVE_DOT = NO

## Generate XML that is required for Breathe
##
GENERATE_XML    = YES
XML_OUTPUT      = xml

GENERATE_HTML   = NO
HAVE_DOT        = NO
GENERATE_LATEX  = NO
GENERATE_MAN    = YES
GENERATE_RTF    = NO

## Skip distracting progress messages
##
QUIET = YES
## Log warnings in a file for further review
##
WARN_LOGFILE = "doxygen-warning-log.txt"