#include "display/lv_display.h" #include "misc/lv_event.h" #include "wifi_board.h" #include "sensecap_audio_codec.h" #include "display/lcd_display.h" #include "application.h" #include "knob.h" #include "config.h" #include "led/single_led.h" #include "power_save_timer.h" #include "sscma_camera.h" #include "dht20.h" #include "mcp_server.h" #include "lvgl_theme.h" #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include "assets/lang_config.h" #define TAG "sensecap_watcher" class CustomLcdDisplay : public SpiLcdDisplay { public: CustomLcdDisplay(esp_lcd_panel_io_handle_t io_handle, esp_lcd_panel_handle_t panel_handle, int width, int height, int offset_x, int offset_y, bool mirror_x, bool mirror_y, bool swap_xy) : SpiLcdDisplay(io_handle, panel_handle, width, height, offset_x, offset_y, mirror_x, mirror_y, swap_xy) { DisplayLockGuard lock(this); auto lvgl_theme = static_cast(current_theme_); auto text_font = lvgl_theme->text_font()->font(); auto icon_font = lvgl_theme->icon_font()->font(); lv_obj_set_size(status_bar_, LV_HOR_RES, text_font->line_height * 2 + 10); lv_obj_set_style_layout(status_bar_, LV_LAYOUT_NONE, 0); lv_obj_set_style_pad_top(status_bar_, 10, 0); lv_obj_set_style_pad_bottom(status_bar_, 1, 0); // 针对圆形屏幕调整位置 // network battery mute // // status // lv_obj_align(battery_label_, LV_ALIGN_TOP_MID, -2.5 * icon_font->line_height, 0); lv_obj_align(network_label_, LV_ALIGN_TOP_MID, -0.5 * icon_font->line_height, 0); lv_obj_align(mute_label_, LV_ALIGN_TOP_MID, 1.5 * icon_font->line_height, 0); lv_obj_align(status_label_, LV_ALIGN_BOTTOM_MID, 0, 0); lv_obj_set_flex_grow(status_label_, 0); lv_obj_set_width(status_label_, LV_HOR_RES * 0.75); lv_label_set_long_mode(status_label_, LV_LABEL_LONG_SCROLL_CIRCULAR); lv_obj_align(notification_label_, LV_ALIGN_BOTTOM_MID, 0, 0); lv_obj_set_width(notification_label_, LV_HOR_RES * 0.75); lv_label_set_long_mode(notification_label_, LV_LABEL_LONG_SCROLL_CIRCULAR); lv_obj_align(low_battery_popup_, LV_ALIGN_BOTTOM_MID, 0, -20); lv_obj_set_style_bg_color(low_battery_popup_, lv_color_hex(0xFF0000), 0); lv_obj_set_width(low_battery_label_, LV_HOR_RES * 0.75); lv_label_set_long_mode(low_battery_label_, LV_LABEL_LONG_SCROLL_CIRCULAR); } }; class SensecapWatcher : public WifiBoard { private: i2c_master_bus_handle_t i2c_bus_; LcdDisplay* display_; std::unique_ptr knob_; esp_io_expander_handle_t io_exp_handle; button_handle_t btns; PowerSaveTimer* power_save_timer_; esp_lcd_panel_io_handle_t panel_io_ = nullptr; esp_lcd_panel_handle_t panel_ = nullptr; uint32_t long_press_cnt_; button_driver_t* btn_driver_ = nullptr; static SensecapWatcher* instance_; SscmaCamera* camera_ = nullptr; DHT20* dht20_sensor_ = nullptr; void InitializePowerSaveTimer() { power_save_timer_ = new PowerSaveTimer(-1, 60, 300); power_save_timer_->OnEnterSleepMode([this]() { GetDisplay()->SetPowerSaveMode(true); GetBacklight()->SetBrightness(10); }); power_save_timer_->OnExitSleepMode([this]() { GetDisplay()->SetPowerSaveMode(false); GetBacklight()->RestoreBrightness(); }); power_save_timer_->OnShutdownRequest([this]() { ESP_LOGI(TAG, "Shutting down"); bool is_charging = (IoExpanderGetLevel(BSP_PWR_VBUS_IN_DET) == 0); if (is_charging) { ESP_LOGI(TAG, "charging"); GetBacklight()->SetBrightness(0); } else { IoExpanderSetLevel(BSP_PWR_SYSTEM, 0); } }); power_save_timer_->SetEnabled(true); } void InitializeI2c() { // Initialize I2C peripheral i2c_master_bus_config_t i2c_bus_cfg = { .i2c_port = (i2c_port_t)0, .sda_io_num = BSP_GENERAL_I2C_SDA, .scl_io_num = BSP_GENERAL_I2C_SCL, .clk_source = I2C_CLK_SRC_DEFAULT, .glitch_ignore_cnt = 7, .intr_priority = 0, .trans_queue_depth = 0, .flags = { .enable_internal_pullup = 1, }, }; ESP_ERROR_CHECK(i2c_new_master_bus(&i2c_bus_cfg, &i2c_bus_)); // pulldown for lcd i2c const gpio_config_t io_config = { .pin_bit_mask = (1ULL << BSP_TOUCH_I2C_SDA) | (1ULL << BSP_TOUCH_I2C_SCL) | (1ULL << BSP_SPI3_HOST_PCLK) | (1ULL << BSP_SPI3_HOST_DATA0) | (1ULL << BSP_SPI3_HOST_DATA1) | (1ULL << BSP_SPI3_HOST_DATA2) | (1ULL << BSP_SPI3_HOST_DATA3) | (1ULL << BSP_LCD_SPI_CS) | (1UL << DISPLAY_BACKLIGHT_PIN), .mode = GPIO_MODE_OUTPUT, .pull_up_en = GPIO_PULLUP_DISABLE, .pull_down_en = GPIO_PULLDOWN_DISABLE, .intr_type = GPIO_INTR_DISABLE, }; gpio_config(&io_config); gpio_set_level(BSP_TOUCH_I2C_SDA, 0); gpio_set_level(BSP_TOUCH_I2C_SCL, 0); gpio_set_level(BSP_LCD_SPI_CS, 0); gpio_set_level(DISPLAY_BACKLIGHT_PIN, 0); gpio_set_level(BSP_SPI3_HOST_PCLK, 0); gpio_set_level(BSP_SPI3_HOST_DATA0, 0); gpio_set_level(BSP_SPI3_HOST_DATA1, 0); gpio_set_level(BSP_SPI3_HOST_DATA2, 0); gpio_set_level(BSP_SPI3_HOST_DATA3, 0); } esp_err_t IoExpanderSetLevel(uint16_t pin_mask, uint8_t level) { return esp_io_expander_set_level(io_exp_handle, pin_mask, level); } uint8_t IoExpanderGetLevel(uint16_t pin_mask) { uint32_t pin_val = 0; esp_io_expander_get_level(io_exp_handle, DRV_IO_EXP_INPUT_MASK, &pin_val); pin_mask &= DRV_IO_EXP_INPUT_MASK; return (uint8_t)((pin_val & pin_mask) ? 1 : 0); } void InitializeExpander() { esp_err_t ret = ESP_OK; esp_io_expander_new_i2c_tca95xx_16bit(i2c_bus_, ESP_IO_EXPANDER_I2C_TCA9555_ADDRESS_001, &io_exp_handle); ret |= esp_io_expander_set_dir(io_exp_handle, DRV_IO_EXP_INPUT_MASK, IO_EXPANDER_INPUT); ret |= esp_io_expander_set_dir(io_exp_handle, DRV_IO_EXP_OUTPUT_MASK, IO_EXPANDER_OUTPUT); ret |= esp_io_expander_set_level(io_exp_handle, DRV_IO_EXP_OUTPUT_MASK, 0); ret |= esp_io_expander_set_level(io_exp_handle, BSP_PWR_SYSTEM, 1); vTaskDelay(100 / portTICK_PERIOD_MS); ret |= esp_io_expander_set_level(io_exp_handle, BSP_PWR_START_UP, 1); vTaskDelay(50 / portTICK_PERIOD_MS); uint32_t pin_val = 0; ret |= esp_io_expander_get_level(io_exp_handle, DRV_IO_EXP_INPUT_MASK, &pin_val); ESP_LOGI(TAG, "IO expander initialized: %x", DRV_IO_EXP_OUTPUT_MASK | (uint16_t)pin_val); assert(ret == ESP_OK); } void OnKnobRotate(bool clockwise) { auto codec = GetAudioCodec(); int current_volume = codec->output_volume(); int new_volume = current_volume + (clockwise ? -5 : 5); // 确保音量在有效范围内 if (new_volume > 100) { new_volume = 100; ESP_LOGW(TAG, "Volume reached maximum limit: %d", new_volume); } else if (new_volume < 0) { new_volume = 0; ESP_LOGW(TAG, "Volume reached minimum limit: %d", new_volume); } codec->SetOutputVolume(new_volume); ESP_LOGI(TAG, "Volume changed from %d to %d", current_volume, new_volume); // 显示通知前检查实际变化 if (new_volume != codec->output_volume()) { ESP_LOGE(TAG, "Failed to set volume! Expected:%d Actual:%d", new_volume, codec->output_volume()); } GetDisplay()->ShowNotification(std::string(Lang::Strings::VOLUME) + ": "+std::to_string(codec->output_volume())); power_save_timer_->WakeUp(); } void InitializeKnob() { knob_ = std::make_unique(BSP_KNOB_A_PIN, BSP_KNOB_B_PIN); knob_->OnRotate([this](bool clockwise) { ESP_LOGD(TAG, "Knob rotation detected. Clockwise:%s", clockwise ? "true" : "false"); OnKnobRotate(clockwise); }); ESP_LOGI(TAG, "Knob initialized with pins A:%d B:%d", BSP_KNOB_A_PIN, BSP_KNOB_B_PIN); } void InitializeButton() { // 设置静态实例指针 instance_ = this; // watcher 是通过长按滚轮进行开机的, 需要等待滚轮释放, 否则用户开机松手时可能会误触成单击 ESP_LOGI(TAG, "waiting for knob button release"); while(IoExpanderGetLevel(BSP_KNOB_BTN) == 0) { vTaskDelay(pdMS_TO_TICKS(50)); } button_config_t btn_config = { .long_press_time = 2000, .short_press_time = 0 }; btn_driver_ = (button_driver_t*)calloc(1, sizeof(button_driver_t)); btn_driver_->enable_power_save = false; btn_driver_->get_key_level = [](button_driver_t *button_driver) -> uint8_t { return !instance_->IoExpanderGetLevel(BSP_KNOB_BTN); }; ESP_ERROR_CHECK(iot_button_create(&btn_config, btn_driver_, &btns)); iot_button_register_cb(btns, BUTTON_SINGLE_CLICK, nullptr, [](void* button_handle, void* usr_data) { auto self = static_cast(usr_data); auto& app = Application::GetInstance(); if (app.GetDeviceState() == kDeviceStateStarting && !WifiStation::GetInstance().IsConnected()) { self->ResetWifiConfiguration(); } self->power_save_timer_->WakeUp(); app.ToggleChatState(); }, this); iot_button_register_cb(btns, BUTTON_LONG_PRESS_START, nullptr, [](void* button_handle, void* usr_data) { auto self = static_cast(usr_data); bool is_charging = (self->IoExpanderGetLevel(BSP_PWR_VBUS_IN_DET) == 0); self->long_press_cnt_ = 0; if (is_charging) { ESP_LOGI(TAG, "charging"); } else { self->IoExpanderSetLevel(BSP_PWR_LCD, 0); self->IoExpanderSetLevel(BSP_PWR_SYSTEM, 0); } }, this); iot_button_register_cb(btns, BUTTON_LONG_PRESS_HOLD, nullptr, [](void* button_handle, void* usr_data) { auto self = static_cast(usr_data); self->long_press_cnt_++; // 每隔20ms加一 // 长按10s 恢复出厂设置: 2+0.02*400 = 10 if (self->long_press_cnt_ > 400) { ESP_LOGI(TAG, "Factory reset"); nvs_flash_erase(); esp_restart(); } }, this); } void InitializeSpi() { ESP_LOGI(TAG, "Initialize SSCMA SPI bus"); spi_bus_config_t spi_cfg = {0}; spi_cfg.mosi_io_num = BSP_SPI2_HOST_MOSI; spi_cfg.miso_io_num = BSP_SPI2_HOST_MISO; spi_cfg.sclk_io_num = BSP_SPI2_HOST_SCLK; spi_cfg.quadwp_io_num = -1; spi_cfg.quadhd_io_num = -1; spi_cfg.isr_cpu_id = ESP_INTR_CPU_AFFINITY_1; spi_cfg.max_transfer_sz = 4095; ESP_ERROR_CHECK(spi_bus_initialize(SPI2_HOST, &spi_cfg, SPI_DMA_CH_AUTO)); ESP_LOGI(TAG, "Initialize QSPI bus"); spi_bus_config_t qspi_cfg = {0}; qspi_cfg.sclk_io_num = BSP_SPI3_HOST_PCLK; qspi_cfg.data0_io_num = BSP_SPI3_HOST_DATA0; qspi_cfg.data1_io_num = BSP_SPI3_HOST_DATA1; qspi_cfg.data2_io_num = BSP_SPI3_HOST_DATA2; qspi_cfg.data3_io_num = BSP_SPI3_HOST_DATA3; qspi_cfg.max_transfer_sz = DISPLAY_WIDTH * DISPLAY_HEIGHT * DRV_LCD_BITS_PER_PIXEL / 8 / CONFIG_BSP_LCD_SPI_DMA_SIZE_DIV; ESP_ERROR_CHECK(spi_bus_initialize(SPI3_HOST, &qspi_cfg, SPI_DMA_CH_AUTO)); } void Initializespd2010Display() { ESP_LOGI(TAG, "Install panel IO"); const esp_lcd_panel_io_spi_config_t io_config = { .cs_gpio_num = BSP_LCD_SPI_CS, .dc_gpio_num = -1, .spi_mode = 3, .pclk_hz = DRV_LCD_PIXEL_CLK_HZ, .trans_queue_depth = 2, .lcd_cmd_bits = DRV_LCD_CMD_BITS, .lcd_param_bits = DRV_LCD_PARAM_BITS, .flags = { .quad_mode = true, }, }; spd2010_vendor_config_t vendor_config = { .flags = { .use_qspi_interface = 1, }, }; esp_lcd_new_panel_io_spi((esp_lcd_spi_bus_handle_t)BSP_LCD_SPI_NUM, &io_config, &panel_io_); ESP_LOGD(TAG, "Install LCD driver"); const esp_lcd_panel_dev_config_t panel_config = { .reset_gpio_num = BSP_LCD_GPIO_RST, // Shared with Touch reset .rgb_ele_order = DRV_LCD_RGB_ELEMENT_ORDER, .bits_per_pixel = DRV_LCD_BITS_PER_PIXEL, .vendor_config = &vendor_config, }; esp_lcd_new_panel_spd2010(panel_io_, &panel_config, &panel_); esp_lcd_panel_reset(panel_); esp_lcd_panel_init(panel_); esp_lcd_panel_mirror(panel_, DISPLAY_MIRROR_X, DISPLAY_MIRROR_Y); esp_lcd_panel_disp_on_off(panel_, true); display_ = new CustomLcdDisplay(panel_io_, panel_, DISPLAY_WIDTH, DISPLAY_HEIGHT, DISPLAY_OFFSET_X, DISPLAY_OFFSET_Y, DISPLAY_MIRROR_X, DISPLAY_MIRROR_Y, DISPLAY_SWAP_XY); // 使每次刷新的起始列数索引是4的倍数且列数总数是4的倍数,以满足SPD2010的要求 lv_display_add_event_cb(lv_display_get_default(), [](lv_event_t *e) { lv_area_t *area = (lv_area_t *)lv_event_get_param(e); uint16_t x1 = area->x1; uint16_t x2 = area->x2; // round the start of area down to the nearest 4N number area->x1 = (x1 >> 2) << 2; // round the end of area up to the nearest 4M+3 number area->x2 = ((x2 >> 2) << 2) + 3; }, LV_EVENT_INVALIDATE_AREA, NULL); } uint16_t BatterygetVoltage(void) { static bool initialized = false; static adc_oneshot_unit_handle_t adc_handle; static adc_cali_handle_t cali_handle = NULL; if (!initialized) { adc_oneshot_unit_init_cfg_t init_config = { .unit_id = ADC_UNIT_1, }; adc_oneshot_new_unit(&init_config, &adc_handle); adc_oneshot_chan_cfg_t ch_config = { .atten = BSP_BAT_ADC_ATTEN, .bitwidth = ADC_BITWIDTH_DEFAULT, }; adc_oneshot_config_channel(adc_handle, BSP_BAT_ADC_CHAN, &ch_config); adc_cali_curve_fitting_config_t cali_config = { .unit_id = ADC_UNIT_1, .chan = BSP_BAT_ADC_CHAN, .atten = BSP_BAT_ADC_ATTEN, .bitwidth = ADC_BITWIDTH_DEFAULT, }; if (adc_cali_create_scheme_curve_fitting(&cali_config, &cali_handle) == ESP_OK) { initialized = true; } } if (initialized) { int raw_value = 0; int voltage = 0; // mV adc_oneshot_read(adc_handle, BSP_BAT_ADC_CHAN, &raw_value); adc_cali_raw_to_voltage(cali_handle, raw_value, &voltage); voltage = voltage * 82 / 20; // ESP_LOGI(TAG, "voltage: %dmV", voltage); return (uint16_t)voltage; } return 0; } uint8_t BatterygetPercent(bool print = false) { int voltage = 0; for (uint8_t i = 0; i < 10; i++) { voltage += BatterygetVoltage(); } voltage /= 10; int percent = (-1 * voltage * voltage + 9016 * voltage - 19189000) / 10000; percent = (percent > 100) ? 100 : (percent < 0) ? 0 : percent; if (print) { printf("voltage: %dmV, percentage: %d%%\r\n", voltage, percent); } return (uint8_t)percent; } void InitializeCmd() { esp_console_repl_t *repl = NULL; esp_console_repl_config_t repl_config = ESP_CONSOLE_REPL_CONFIG_DEFAULT(); repl_config.max_cmdline_length = 1024; repl_config.prompt = "SenseCAP>"; const esp_console_cmd_t cmd1 = { .command = "reboot", .help = "reboot the device", .hint = nullptr, .func = [](int argc, char** argv) -> int { esp_restart(); return 0; }, .argtable = nullptr }; ESP_ERROR_CHECK(esp_console_cmd_register(&cmd1)); const esp_console_cmd_t cmd2 = { .command = "shutdown", .help = "shutdown the device", .hint = nullptr, .func = NULL, .argtable = NULL, .func_w_context = [](void *context,int argc, char** argv) -> int { auto self = static_cast(context); self->GetBacklight()->SetBrightness(0); self->IoExpanderSetLevel(BSP_PWR_SYSTEM, 0); return 0; }, .context =this }; ESP_ERROR_CHECK(esp_console_cmd_register(&cmd2)); const esp_console_cmd_t cmd3 = { .command = "battery", .help = "get battery percent", .hint = NULL, .func = NULL, .argtable = NULL, .func_w_context = [](void *context,int argc, char** argv) -> int { auto self = static_cast(context); self->BatterygetPercent(true); return 0; }, .context =this }; ESP_ERROR_CHECK(esp_console_cmd_register(&cmd3)); const esp_console_cmd_t cmd4 = { .command = "factory_reset", .help = "factory reset and reboot the device", .hint = NULL, .func = NULL, .argtable = NULL, .func_w_context = [](void *context,int argc, char** argv) -> int { nvs_flash_erase(); esp_restart(); return 0; }, .context =this }; ESP_ERROR_CHECK(esp_console_cmd_register(&cmd4)); const esp_console_cmd_t cmd5 = { .command = "read_mac", .help = "Read mac address", .hint = NULL, .func = NULL, .argtable = NULL, .func_w_context = [](void *context,int argc, char** argv) -> int { uint8_t mac[6]; esp_read_mac(mac, ESP_MAC_WIFI_STA); printf("wifi_sta_mac: " MACSTR "\n", MAC2STR(mac)); esp_read_mac(mac, ESP_MAC_WIFI_SOFTAP); printf("wifi_softap_mac: " MACSTR "\n", MAC2STR(mac)); esp_read_mac(mac, ESP_MAC_BT); printf("bt_mac: " MACSTR "\n", MAC2STR(mac)); return 0; }, .context =this }; ESP_ERROR_CHECK(esp_console_cmd_register(&cmd5)); const esp_console_cmd_t cmd6 = { .command = "version", .help = "Read version info", .hint = NULL, .func = NULL, .argtable = NULL, .func_w_context = [](void *context,int argc, char** argv) -> int { auto self = static_cast(context); auto app_desc = esp_app_get_description(); const char* region = "UNKNOWN"; #if defined(CONFIG_LANGUAGE_ZH_CN) region = "CN"; #elif defined(CONFIG_LANGUAGE_EN_US) region = "US"; #elif defined(CONFIG_LANGUAGE_JA_JP) region = "JP"; #elif defined(CONFIG_LANGUAGE_ES_ES) region = "ES"; #elif defined(CONFIG_LANGUAGE_DE_DE) region = "DE"; #elif defined(CONFIG_LANGUAGE_FR_FR) region = "FR"; #elif defined(CONFIG_LANGUAGE_IT_IT) region = "IT"; #elif defined(CONFIG_LANGUAGE_PT_PT) region = "PT"; #elif defined(CONFIG_LANGUAGE_RU_RU) region = "RU"; #elif defined(CONFIG_LANGUAGE_KO_KR) region = "KR"; #endif printf("{\"type\":0,\"name\":\"VER?\",\"code\":0,\"data\":{\"software\":\"%s\",\"hardware\":\"watcher xiaozhi agent\",\"camera\":%d,\"region\":\"%s\"}}\n", app_desc->version, self->GetCamera() == nullptr ? 0 : 1, region); return 0; }, .context =this }; ESP_ERROR_CHECK(esp_console_cmd_register(&cmd6)); esp_console_dev_uart_config_t hw_config = ESP_CONSOLE_DEV_UART_CONFIG_DEFAULT(); ESP_ERROR_CHECK(esp_console_new_repl_uart(&hw_config, &repl_config, &repl)); ESP_ERROR_CHECK(esp_console_start_repl(repl)); } void InitializeCamera() { ESP_LOGI(TAG, "Initialize Camera"); // !!!NOTE: SD Card use same SPI bus as sscma client, so we need to disable SD card CS pin first const gpio_config_t io_config = { .pin_bit_mask = (1ULL << BSP_SD_SPI_CS), .mode = GPIO_MODE_OUTPUT, .pull_up_en = GPIO_PULLUP_ENABLE, .pull_down_en = GPIO_PULLDOWN_DISABLE, .intr_type = GPIO_INTR_DISABLE, }; esp_err_t ret = gpio_config(&io_config); if (ret != ESP_OK) return; gpio_set_level(BSP_SD_SPI_CS, 1); camera_ = new SscmaCamera(io_exp_handle); } void InitializeDHT20() { ESP_LOGI(TAG, "Initialize DHT20 sensor on Grove port"); // Create DHT20 sensor instance dht20_sensor_ = new DHT20(i2c_bus_); // Initialize and calibrate the sensor esp_err_t ret = dht20_sensor_->Initialize(); if (ret != ESP_OK) { ESP_LOGE(TAG, "DHT20 initialization failed: %s", esp_err_to_name(ret)); delete dht20_sensor_; dht20_sensor_ = nullptr; return; } ESP_LOGI(TAG, "DHT20 sensor initialized successfully"); // Register MCP tool for reading temperature and humidity auto& mcp_server = McpServer::GetInstance(); mcp_server.AddTool("self.grove.get_temperature_humidity", "从Grove接口的DHT20传感器读取温湿度数据\n" "返回格式: {\"temperature\": 温度值(°C), \"humidity\": 湿度值(%), \"status\": \"ok\"}\n" "如果读取失败,返回错误信息", PropertyList(), [this](const PropertyList&) -> ReturnValue { if (!dht20_sensor_) { return "{\"error\": \"DHT20 sensor not initialized\"}"; } float temperature = 0.0f; float humidity = 0.0f; esp_err_t ret = dht20_sensor_->ReadTempAndHumidity(temperature, humidity); if (ret != ESP_OK) { std::string error_msg = "{\"error\": \"Failed to read DHT20: "; error_msg += esp_err_to_name(ret); error_msg += "\"}"; return error_msg; } // Format response as JSON char buffer[128]; snprintf(buffer, sizeof(buffer), "{\"temperature\": %.2f, \"humidity\": %.2f, \"status\": \"ok\"}", temperature, humidity); return std::string(buffer); }); ESP_LOGI(TAG, "DHT20 MCP tool registered: self.grove.get_temperature_humidity"); } public: SensecapWatcher() { ESP_LOGI(TAG, "Initialize Sensecap Watcher"); InitializePowerSaveTimer(); InitializeI2c(); InitializeSpi(); InitializeExpander(); InitializeCmd(); //工厂生产测试使用 InitializeButton(); InitializeKnob(); Initializespd2010Display(); GetBacklight()->RestoreBrightness(); // 对于不带摄像头的版本,InitializeCamera需要3s, 所以先恢复背光亮度 InitializeCamera(); InitializeDHT20(); // Initialize Grove DHT20 sensor } virtual AudioCodec* GetAudioCodec() override { static SensecapAudioCodec audio_codec( i2c_bus_, AUDIO_INPUT_SAMPLE_RATE, AUDIO_OUTPUT_SAMPLE_RATE, AUDIO_I2S_GPIO_MCLK, AUDIO_I2S_GPIO_BCLK, AUDIO_I2S_GPIO_WS, AUDIO_I2S_GPIO_DOUT, AUDIO_I2S_GPIO_DIN, AUDIO_CODEC_PA_PIN, AUDIO_CODEC_ES8311_ADDR, AUDIO_CODEC_ES7243E_ADDR, AUDIO_INPUT_REFERENCE); return &audio_codec; } virtual Display* GetDisplay() override { return display_; } virtual Backlight* GetBacklight() override { static PwmBacklight backlight(DISPLAY_BACKLIGHT_PIN, DISPLAY_BACKLIGHT_OUTPUT_INVERT); return &backlight; } // 根据 https://github.com/Seeed-Studio/OSHW-SenseCAP-Watcher/blob/main/Hardware/SenseCAP_Watcher_v1.0_SCH.pdf // RGB LED型号为 ws2813 mini, 连接在GPIO 40,供电电压 3.3v, 没有连接 BIN 双信号线 // 可以直接兼容SingleLED采用的ws2812 virtual Led* GetLed() override { static SingleLed led(BUILTIN_LED_GPIO); return &led; } virtual void SetPowerSaveMode(bool enabled) override { if (!enabled) { power_save_timer_->WakeUp(); } WifiBoard::SetPowerSaveMode(enabled); } virtual bool GetBatteryLevel(int &level, bool& charging, bool& discharging) override { static bool last_discharging = false; charging = (IoExpanderGetLevel(BSP_PWR_VBUS_IN_DET) == 0); discharging = !charging; level = (int)BatterygetPercent(false); if (discharging != last_discharging) { power_save_timer_->SetEnabled(discharging); last_discharging = discharging; } if (level <= 1 && discharging) { ESP_LOGI(TAG, "Battery level is low, shutting down"); IoExpanderSetLevel(BSP_PWR_SYSTEM, 0); } return true; } virtual Camera* GetCamera() override { return camera_; } }; DECLARE_BOARD(SensecapWatcher); // 定义静态成员变量 SensecapWatcher* SensecapWatcher::instance_ = nullptr;